STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! GPIO port documentation query: P-MOS is shown inverted but is active high, and vice versa for N-MOS

With reference to RM0436, the STM32MP157 Reference Manual, revision 6.On pages 1066 and 1072 the schematic structures of a GPIO port are drawn (figures 119, 120, and 122). These all show an inverter circle on the gate of P-MOS output transistor and n...

tarmasr by Associate III
  • 3151 Views
  • 2 replies
  • 0 kudos

What is the highest version of opencv compatible with the gstreamer library included in this SDK?

I have transplanted the latest opencv-4.8.1 on the STM32MP135F-DK Discovery Board and run a program to capture video stream from a camera on the borad.I found if I cmake the opencv-4.8.1 source code with "-DWITH_GSTREAMER=ON -DBUILD_GSTREAMER=ON",and...

babai50 by Associate
  • 2294 Views
  • 1 replies
  • 0 kudos

Resolved! change OpenST Linux version in STM32CubeMX

We are using developBoard by Emcraft with STM32MP157A.Emcraft release board with Openstlinux 4.14. If I want change devicetree of STM32MP1 i need use STM32CubeMX to export new devicetree.If i go in STM32CubeMX-->Project Manager-> Project OpenSTLinux ...

AApol.3 by Associate
  • 2939 Views
  • 5 replies
  • 0 kudos

STLINK-V3PWR feedback

Not sure if this is the right place to write this, but I cannot help to write:- STLINK-V3PWR is a great tool.- I wish it had an external power input other than USB-C. It may be common in some computer setups, but powered USB ports might be challengin...

mete by Senior II
  • 1694 Views
  • 1 replies
  • 3 kudos