STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32MP157FAD schematic design

hiI am working on a project using stm32mp157fad.For the project created using stm32cubemx and stm32cubeide, I created a custom image by referring to the site below and uploaded it to the sd card using the dd command.But openstlinux is not booting up ...

_legacyfs_online_stmicro_images_0693W00000bkVSlQAM.png _legacyfs_online_stmicro_images_0693W00000bkVTsQAM.png
KNam.2 by Associate II
  • 1973 Views
  • 4 replies
  • 0 kudos

Resolved! eMMC HS200 clarification

Hi there,we are in the process of developing a product based on the STM32MP151F which will be USB powered (USB 2.0 device).We are aiming to have it connected to an eMMC for mass storage and we would like to achive the highest R/W speed which should b...

Resolved! Can't flash SD card on STM32MP157-EVAL

I have a STM32MP15X-EVAL board MB1262C-01 with a MB1263B-04 CPU-board on it (MP157AAA3). I'm following the instructions from 'STM32MP15_Evaluation_boards_-_Starter_Package'Boot 0,1,2 jumpers are OFF, JP1 is removed. USB connected to CN4 (ST-Link) an...

NKall.1 by Associate II
  • 1997 Views
  • 4 replies
  • 0 kudos

Resolved! Stm32mp157 Programming NOR flash

Trying to load TF-A and uboot into NOR flash, but I always get this error.SF: Detected w25q256 with page size 256 Bytes, erase size 64 KiB, total 32 MiBmtdids=nor0=nor0 & mtdparts=mtdparts=nor0:256k(fsbl1),256k(fsbl2),2m(ssbl),512k(u-boot-env),-(nor_...

uouox by Associate II
  • 1127 Views
  • 2 replies
  • 0 kudos