STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32MP151C SPI5 clock much slower

I am trying to configure SPI5 on STM32MP151C where MPU is a master and ESP32C6 is a slave. The clock used in the device tree is HSI 64MHz. SPI driver is running with 2MHz configured and divisor in the SPI_CFG1 register is correctly set to 32. In the ...

vsaakian by Associate III
  • 3528 Views
  • 2 replies
  • 1 kudos

STM32MP153 - How to enable HSI clock?

Hi, I set MCO1 using HSE clock and get 8MHz working well (my HSE is 8MHz)But I need 16MHz or higher on MCO1, so I changed to MCO1 source clock by HSI but there is nothing.I tested other CSI, HSE, ... MCO1 work, except for HSI.I think there is somethi...

Dat Tran by Senior II
  • 1628 Views
  • 1 replies
  • 0 kudos

Issue regarding DDR3

HelloI'm using stm32mp157aaa3 processor in our custom board.And I'm working on DDR3L with arm-trusted-firmware(V2.5) ddr3 routines as my reference code and reference manual(RM0436) and Application not(AN5168).When I am hard-coding the register values...

m4projects-stm32mp1-1.6.0 fetcher failure

Hi,I'm trying to build core-image-minimal yocto project for my STM32MP157D-DK1 board according to digikey tutorial and I stuck at fetching m4projects dependency. Does anybody faces and resolved this issue?My build conf:Build Configuration:BB_VERSION ...

dnj by Associate III
  • 1601 Views
  • 0 replies
  • 0 kudos

Resolved! TF-A hangs on stm32mp157d-dk1

Hello all, As part of the evaluation of the 32MP15 series, I was trying to build the u-boot and TF-A binaries. I tried the u-boot SPL bring up and it seems to be working fine (except for failure to launch the Linux Kernel, as per your late updates). ...

Resolved! STM32MP131FAF7T how to program PMIC

I have a custom built  STM32MP131FAF7T board and can't set my VOUT2. The only line that is down is my VDD DDR Lines since I can't program my PMIC (STPMIC1DPQR) to have the VOUT2 to be 1.35 volts instead of 1.1 volts. My VCPU is at 1.2V, VDD is at  3....

T_Dodd by Associate
  • 1996 Views
  • 1 replies
  • 0 kudos

Resolved! Building kernel image and device tree

Hey, I'm following the Getting started tutorial and have some troubles at the chapter "Modify, rebuild and reload the Linux kernel":https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157x-DK2/Develop_on_Arm%C2%AE_Cortex%C2%AE-A7...

oli1 by Associate II
  • 3011 Views
  • 2 replies
  • 1 kudos

DCMI resolution on STM32MP157c ?

I'm trying to use an ADV7280 videodecoder with DCMI and embedded linux on a board based on STM32157c-dk2. The decoder should output 720x576 picture resolution with the camera (PAL,CV) attached. However the DCMI seems to be in 'normal mode' which allo...

Ronte.1 by Associate III
  • 4770 Views
  • 7 replies
  • 0 kudos