STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! FDCAN in normal mode is not working

Hi!I am using the stm32mp157C-DK2 board to communicate via FDCAN and my idea is to use it as normal mode to send and receive CAN messages. For this I have created a program in stm32cubeide and I enable FDCAN1 with the following parameters (125Kb/s): ...

TArre.1 by Associate III
  • 3324 Views
  • 7 replies
  • 0 kudos

I can not find any 8 gigabit memory for the STM32MP157CAA3 What I have found is double the price of the processor! IS46TR16512BL ISSI and Micron ECF840AAACN-C1-Y3

I can not find any 8 gigabit memory for the STM32MP157CAA3 What I have found is double the price of the processor! IS46TR16512BL ISSI and Micron ECF840AAACN-C1-Y3I was looking for 256X32 memory but gave up, found some 512X16 but this puts the the cos...

KevinA by Senior
  • 1814 Views
  • 7 replies
  • 0 kudos

Resolved! USB PHY issue in STM32mp157A

Hello,I am working on a custom board based on STM32MP157A and I am getting all the bits correctly but getting values at reserved bits in USBPHYC version register (Internal) which are supposed to be reserved  as per the reference manual.Below mentione...

USBPHYC_ReferenceManual.png Screenshot from 2023-12-05 17-24-39.png