STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32MP157 unable to boot from SD

As part of our project, we are using an STM32MP157DAC custom board that has the same design with the STM32MP157D-DK1 development board except for a few changes (schematics of the design is attached)The board generally works when trying to upload and ...

shobole by Associate
  • 2954 Views
  • 2 replies
  • 0 kudos

Resolved! uint8_t Values Are Not Changing

 I want to download and use firmware (FW) to DDR3. Since DDR is initially disabled, the firmware to activate DDR and the main FW project are separate, and the download procedure is as follows:First, run the DDR activation FW to enable DDR.Download th...

Stnoobs by Associate II
  • 6356 Views
  • 12 replies
  • 0 kudos