STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32MP131 waiting for UUID

Hi everyone, I made it past the bootloader stages but am now running into errors with starting the Linux kernel. I have an eMMC and SD card but I am trying to only use the SD card for now. I have completely removed the eMMC from device tree and remov...

Resolved! OPTEE-OS DTS for STM32MP131D

Hi everyone, I am trying to boot up a custom PCB using the STM32MP131D, however I am running into an error during OPTEE. I have attached the optee dts and also a debug log of OPTEE during boot. I confirmed that sdmmc1_io, sdmmc2_io, and cpu0_opp_tabl...

scp failure

I was going through the "Modify, rebuild and reload the Linux® kernel" section of the getting started guide for the STM32MP157x-DK2 board:https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157x-DK2/Develop_on_Arm%C2%AE_Cortex%C2...

Install pip3-install

  Hi,I have a STM32MP157F-DK2 and I can't install anything on the card, especially python3-pip, obviously the card is correctly connected to the internet via ethernet and the date and time are correct.I tried both with:- ap-get update- apt-get upgrad...

Delios82 by Associate II
  • 1339 Views
  • 0 replies
  • 0 kudos