STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32MP157C-DK2 Uart Boot

Is it possible to boot over UART on the STM32MP157C-DK2? I set the BOOT pins as following:BOOT0 - OFFBOOT1 - OFFI am using the FT232 UART-USB Adapter and have connected the following pins:UART GND - CN16 GNDUART VCC - CN16 3.3VUART TX - CN14 ARD_D1UA...

ANiko.3 by Associate II
  • 7656 Views
  • 14 replies
  • 0 kudos

Complex Project idea on STM32MP1 DK2?

I am working on STM32MP1 DK2 as a Hobby Project, can anyone suggest me a complex project to get to a linux + RTOS based project developement. I want to get an hands on idea on RTOS + Linux project. I saw a video of Zephyr project with Intel which ran...

sanket47 by Associate II
  • 1795 Views
  • 1 replies
  • 1 kudos

STLinux Ecosystem v2 boot chain problems.

We have a custom board based on the STM32MP157 series, and are trying to get the TF-A boot chain working.  We have downloaded and compiled the linux kernel, u-boot, and arm-trusted-firmware for the STLinux ecosystem v2.  We can boot to u-boot, and th...

Macdog by Associate III
  • 1587 Views
  • 1 replies
  • 0 kudos

Resolved! Key format for secure boot

Hi, I'm trying to generate secure boot keys using native linux tools. I assumed the secureboot format would be documented, but all I found was links to STM32MP_KeyGen.I can use openssl to generate ECDSA keys, and also get publik keys out. I am at teh...

mrnuke by Associate II
  • 1637 Views
  • 1 replies
  • 0 kudos

Resolved! How can I prevent the contents of "RETRAM" from being erased? (base on linux with m4 rproc)

Hi all.I want to prevent the contents of "RETRAM" from being erased when I run the firmware with m4 rproc on "OpenSTLinux"."RETRAM" is powered by the battery through the VBAT pin to maintain data.To this end, TF-A was also modified to set and maintai...

Machilus by Associate III
  • 1915 Views
  • 3 replies
  • 0 kudos

Resolved! No wlan0 on DK1 I just received.

I have a pair of DK1 boards I just received that I wanted to get working with wifi direct, but neither even can show a wlan0 interface. In the past I have used a DK2 with buildroot and got the wlan0, and a coworker used stock yocto build on the DK2 a...

BillR by Senior
  • 1367 Views
  • 1 replies
  • 0 kudos