cancel
Showing results for 
Search instead for 
Did you mean: 

CCM in stm32mp157

AMART.1
Associate

Hi all,

If I dedicate the MCU SRAM2 for data and MCU SRAM4 for DMA as shown here, do I get CCM like performance or do I have a risk to have contention on the SRAM2 ?

After looking at the bus matrix, I suspect there is no risk but I want to make sure it is the case.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
PatrickF
ST Employee

I confirm there is no contention in the MLAHB matrix, e.g. in your case between Cortex-M4 and SRAM2 and DMA access to SRAM4.

For information, to get best performances for Cortex-M4 DATA access, either RETRAM (@0x00000000, using D-Bus) or SRAM2 alias (@0x30020000, using S-Bus) should be used (other SRAMs have still good performances, but could have 1 additional wait-state on non-sequential access from Cortex-M4). Notice that Cortex-M4 INSTRUCTION fetch is 'optimized' on either S-bus or I-bus on all SRAMs and RETRAM (even if I-bus should be preferable).

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here

View solution in original post

2 REPLIES 2
PatrickF
ST Employee

I confirm there is no contention in the MLAHB matrix, e.g. in your case between Cortex-M4 and SRAM2 and DMA access to SRAM4.

For information, to get best performances for Cortex-M4 DATA access, either RETRAM (@0x00000000, using D-Bus) or SRAM2 alias (@0x30020000, using S-Bus) should be used (other SRAMs have still good performances, but could have 1 additional wait-state on non-sequential access from Cortex-M4). Notice that Cortex-M4 INSTRUCTION fetch is 'optimized' on either S-bus or I-bus on all SRAMs and RETRAM (even if I-bus should be preferable).

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here
AMART.1
Associate

Hi @PatrickF​ ,

Thanks for the detailed explanation.