STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Build image linux-stm32mp-5.4.56-r0

Hello totgehet,i wanted to build a Kernelmodule for my Projekt so i started to install the SDK and wrote a simple Programm to see if i can make a Programm in the userspace. This works fine. My next step was to Building and deploying the Linux kernel....

SAman.1 by Associate III
  • 2214 Views
  • 3 replies
  • 0 kudos

Error trying to build dtb

Hi, I tried to follow the example in the youtube workshop, moving a pwm timer to the a7 side. I was able to create a dts file with cube mx but when running make to build the dtb i get"reference to non existent node or label "ethernet_mac_address""Is ...

OHaza.1 by Associate III
  • 1340 Views
  • 2 replies
  • 0 kudos

How to disable VREFBUF and supply external VREF for ADC (which is assigned to M4 runtime context)?

Hi,I need to supply external VREF for ADC which is assigned to M4 runtime context. Now when I start M4 firmware VREFBUF is activated (I'm measuring 2.5V on AVDD pin on DK2 kit). I suppose that I need to edit device tree, but I'm not sure. Can I for e...

NGajic by Associate III
  • 2365 Views
  • 2 replies
  • 0 kudos