cancel
Showing results for 
Search instead for 
Did you mean: 

STM32MP1 STM32CubeProgramming Unable to reconnect the target device time out expired

MVENN.1
Associate II

Hi ,

I am using STM32MP157C-DK2 board

I just trying to load the flash image in to the SD card.

facing issue reconnecting the device. Below i mentioned log file please check it.

 10:04:18 : STM32CubeProgrammer API v 2.6.0

 10:05:47 : Error: No debug probe detected.

 10:06:19 : Error: No debug probe detected.

 10:06:34 : USB speed  : High Speed (480MBit/s)

 10:06:34 : Manuf. ID  : 

 10:06:34 : Product ID : 

 10:06:34 : SN     : 

 10:06:34 : FW version : 0x0110

 10:06:34 : IAP

 10:06:35 : UPLOADING ...

 10:06:35 :  Size     : 1024 Bytes

 10:06:35 :  Address    : 0x8000000

 10:06:35 : Read progress:

 10:06:35 : Error: Data read failed

 10:06:47 : Disconnected from device.

 10:07:17 : USB speed  : High Speed (480MBit/s)

 10:07:17 : Manuf. ID  : 

 10:07:17 : Product ID : 

 10:07:17 : SN     : 

 10:07:17 : FW version : 0x0110

 10:07:17 : IAP

 10:07:18 : UPLOADING ...

 10:07:18 :  Size     : 1024 Bytes

 10:07:18 :  Address    : 0x8000000

 10:07:18 : Read progress:

 10:07:18 : Error: Data read failed

 10:07:28 : Disconnected from device.

 10:08:00 : USB speed  : High Speed (480MBit/s)

 10:08:00 : Manuf. ID  : STMicroelectronics

 10:08:00 : Product ID : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000

 10:08:00 : SN     : 0034001A3438510438333630

 10:08:00 : FW version : 0x0110

 10:08:00 : Device ID  : 0x0500

 10:08:28 : Read TSV File: /home/moveon/STM32MPU_workspace/STM32MP15-Ecosystem-v2.1.0/Starter-Package/stm32mp1-openstlinux-5-4-dunfell-mp1-20-11-12/images/stm32mp1/flashlayout_st-image-weston/trusted/FlashLayout_sdcard_stm32mp157c-dk2-trusted.tsv

 10:08:28 : Number of partitions: 9

 10:08:50 : Start Embedded Flashing service

 10:08:50 : Memory Programming ...

 10:08:50 : Opening and parsing file: tf-a-stm32mp157c-dk2-serialboot.stm32

 10:08:50 :  File     : tf-a-stm32mp157c-dk2-serialboot.stm32

 10:08:50 :  Size     : 237896 Bytes

 10:08:50 :  Partition ID : 0x01 

 10:08:50 : Download in Progress:

 10:08:51 : File download complete

 10:08:51 : Time elapsed during download operation: 00:00:00.651

 10:08:51 : RUNNING Program ... 

 10:08:51 :  PartID:   :0x01 

 10:08:51 : Start operation done successfully at partition 0x01

 10:08:51 : Flashlayout Programming ...

 10:08:51 : Running Flashlayout Partition ...

 10:08:51 : Flashlayout partition started successfully

 10:08:51 : Memory Programming ...

 10:08:51 : Opening and parsing file: u-boot-stm32mp157c-dk2-trusted.stm32

 10:08:51 :  File     : u-boot-stm32mp157c-dk2-trusted.stm32

 10:08:51 :  Size     : 904820 Bytes

 10:08:51 :  Partition ID : 0x03 

 10:08:51 : Download in Progress:

 10:08:53 : File download complete

 10:08:53 : Time elapsed during download operation: 00:00:01.684

 10:08:53 : RUNNING Program ... 

 10:08:53 :  PartID:   :0x03 

 10:08:53 : reconnecting the device ...

 10:09:10 : USB speed  : High Speed (480MBit/s)

 10:09:10 : Manuf. ID  : STMicroelectronics

 10:09:10 : Product ID : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000

 10:09:10 : SN     : 0034001A3438510438333630

 10:09:10 : FW version : 0x0110

 10:09:10 : Device ID  : 0x0500

 10:09:10 : Start operation done successfully at partition 0x03

 10:09:10 : Memory Programming ...

 10:09:10 : Opening and parsing file: tf-a-stm32mp157c-dk2-serialboot.stm32

 10:09:10 :  File     : tf-a-stm32mp157c-dk2-serialboot.stm32

 10:09:10 :  Size     : 237896 Bytes

 10:09:10 :  Partition ID : 0x01 

 10:09:10 : Download in Progress:

 10:09:11 : File download complete

 10:09:11 : Time elapsed during download operation: 00:00:00.888

 10:09:11 : RUNNING Program ... 

 10:09:11 :  PartID:   :0x01 

 10:09:11 : Start operation done successfully at partition 0x01

 10:09:11 : Flashlayout Programming ...

 10:09:11 : Running Flashlayout Partition ...

 10:09:11 : Flashlayout partition started successfully

 10:09:11 : Memory Programming ...

 10:09:11 : Opening and parsing file: u-boot-stm32mp157c-dk2-trusted.stm32

 10:09:11 :  File     : u-boot-stm32mp157c-dk2-trusted.stm32

 10:09:11 :  Size     : 904820 Bytes

 10:09:11 :  Partition ID : 0x03 

 10:09:11 : Download in Progress:

 10:09:13 : File download complete

 10:09:13 : Time elapsed during download operation: 00:00:01.717

 10:09:13 : RUNNING Program ... 

 10:09:13 :  PartID:   :0x03 

 10:09:13 : reconnecting the device ...

 10:09:31 : USB speed  : High Speed (480MBit/s)

 10:09:31 : Manuf. ID  : STMicroelectronics

 10:09:31 : Product ID : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000

 10:09:31 : SN     : 0034001A3438510438333630

 10:09:31 : FW version : 0x0110

 10:09:31 : Device ID  : 0x0500

 10:09:31 : Start operation done successfully at partition 0x03

 10:09:31 : Memory Programming ...

 10:09:31 : Opening and parsing file: tf-a-stm32mp157c-dk2-serialboot.stm32

 10:09:31 :  File     : tf-a-stm32mp157c-dk2-serialboot.stm32

 10:09:31 :  Size     : 237896 Bytes

 10:09:31 :  Partition ID : 0x01 

 10:09:31 : Download in Progress:

 10:09:32 : File download complete

 10:09:32 : Time elapsed during download operation: 00:00:00.757

 10:09:32 : RUNNING Program ... 

 10:09:32 :  PartID:   :0x01 

 10:09:32 : Start operation done successfully at partition 0x01

 10:09:32 : Flashlayout Programming ...

 10:09:32 : Running Flashlayout Partition ...

 10:09:32 : Flashlayout partition started successfully

 10:09:32 : Memory Programming ...

 10:09:32 : Opening and parsing file: u-boot-stm32mp157c-dk2-trusted.stm32

 10:09:32 :  File     : u-boot-stm32mp157c-dk2-trusted.stm32

 10:09:32 :  Size     : 904820 Bytes

 10:09:32 :  Partition ID : 0x03 

 10:09:32 : Download in Progress:

 10:09:35 : File download complete

 10:09:35 : Time elapsed during download operation: 00:00:01.639

 10:09:35 : RUNNING Program ... 

 10:09:35 :  PartID:   :0x03 

 10:09:35 : reconnecting the device ...

 10:10:04 : Error: Unable to reconnect the target device: time out expired

 10:10:04 : Error: Start operation failed at partition 0x03

 10:10:05 : Error: TSV flashing service failed

 10:10:05 : Warning: Connection to device 0x500 is lost

 10:10:07 : Disconnected from device.

This discussion is locked. Please start a new topic to ask your question.
7 REPLIES 7
KnarfB
Super User

Works for me.

How did you enter DFU mode? What is the boot pins setting? You can hook-up a terminal prog via ST-LINK serial port and some boot log info from inside.

MVENN.1
Associate II

Hi KnarfB(Community Member)

Thanks for reply.

boot pins are off only.ST- L INK serial port is not showing device ID.

please check below one0693W000005CZKoQAO.jpg.0693W000005CZKFQA4.jpg

Please suggest the how to solve this issue.

PatrickF
ST Employee

Hello,

may I suggest you to read this FAQ: https://community.st.com/s/article/FAQ-STM32MP1-STM32CubeProgrammer-USB-reconnect-error-at-STM32MP1-boot-device-flashing

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here

Hi PatrickF( ST Employee )

when i am given this command dmesg it showing

[26478.877667] usb 1-2: new high-speed USB device number 30 using xhci_hcd

[26479.363719] usb 1-2: New USB device found, idVendor=0483, idProduct=df11, bcdDevice= 2.00

[26479.363723] usb 1-2: New USB device strings: Mfr=1, Product=2, SerialNumber=3

[26479.363726] usb 1-2: Product: USB download gadget@Device ID /0x500, @Revision ID /0x2000, @Name /STM32MP157CAC Rev.B,

[26479.363729] usb 1-2: Manufacturer: STMicroelectronics

[26479.363732] usb 1-2: SerialNumber: 0034001A3438510438333630

[26516.580117] usb 1-2: USB disconnect, device number 30

I am not using USB OTG cable just i am using Typle c cable to my PC.

little bit I understand. Please guide me how to solve this issue.

Thanks.

shane mattner
Senior

Check to see if you have this folder on the target:

/lib/firmware

One problem I had is that Buildroot wasn't making a /lib/firmware folder so I could never download/debug.

your flash download seems ok, so if you reset the board, it should fly.

Best is to look at the console (ST-Link VCP) during boot.

Maybe a too weak supply (1A is barely ok, 2A is the minimum, 3A is recommended)

Could you please followup on https://community.st.com/s/question/0D73W000000VPAS to avoid two parallel discussion thread ?

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here