STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Dual Display Support

Hi,Is STM32MP1 is able to drive two displays at once , one via DSI and another via RGB is it possible? Following are the combinations :RGB to HDMI ---- to drive HDMI display.DSI to HDMI ----- to drive HDMI display.RGB to LVDS ----- to Drive LVDS disp...

NPal.2 by Senior
  • 2512 Views
  • 6 replies
  • 0 kudos

Minimal OpenSTLinux

We are building a custom embedded system based on STM32MP1 using customised OpenSTLinux. We are currently using the st-image-core as a starting point but we found it already heavy.Is there any option or other images providing a smaller image ?Also h...

PGE by Associate III
  • 5128 Views
  • 8 replies
  • 0 kudos

Resolved! OpenSTLinux remove wifi and bluetooth support

We are using OpenSTLinux to generate a custom image for our custom board. This board has no wifi nor bluetooth so we would like to remove it's support.Our machine conf file is based on stm32mp1-eval.conf with the following edition (commenting wifi an...

PGE by Associate III
  • 2380 Views
  • 2 replies
  • 0 kudos

Location of generated dtb file.

Hi,I am trying to develop something around the STM32MP1.For that I have made some changes in the dts file via cubeMx and followed the process of building it given here.What is the location where the dtb file generated ? My arch/arm/boot/dts folder lo...

NPal.2 by Senior
  • 3275 Views
  • 3 replies
  • 0 kudos

STM32mp1 pin mux in kernel dts

currently i have a pin <STM32_PINMUX('F', 14, GPIO)> how to mux as a GPIO before using as a gpiolib, export work fine, but i2c4 is not working but i can see GPIO is getting based on sys gpiolib. as before export i see PF14 line is muxed as pin 94 (P...

Ara.1 by Senior
  • 1818 Views
  • 5 replies
  • 0 kudos

How do i run a custom built DDR_Test_Suite (U-Boot.SPL.STM32MP157C-DK2.stm32) using CubeMX?

I am trying to verify my build environment by building the U-boot code samples to be able to run the DDR Tuning tests.First I start CubeMX (using the ubuntu image provided on one of your workshops) and under tools i choose the DDR Test Suite and sele...

DOlss.1 by Associate II
  • 4831 Views
  • 6 replies
  • 3 kudos

Resolved! It's possible to make work USB-OTG and USART1 in the same device (STM32MP157CAC)?

Hi everyone.I have an already-designed PCB with an STM32MP157 on it. In order to communicate with an external device, I am using USART1. At the same time, I'm using an USB OTG port to connect my device to my PC.My problem is that USART1 is working wi...

areify by Associate II
  • 13150 Views
  • 12 replies
  • 0 kudos