STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Device not Detected using JLink

I am using a custom.board with STM32MP157C.I am not able to connect to it via JLink EDU.It shows that the ST device could not be verified.Also tried using the STM32Cube ide as well as JLink commander.Facing same issue.What should I give in the device...

KS.2 by Associate III
  • 5720 Views
  • 4 replies
  • 0 kudos

L2CAP Bluetooth: message too long

Hi everyone,I want to send messages with L2CAP protocol between two Bluetooth devices. This is my client code:void process_bluetooth () {   int bl_buff_it = 0; // global buffer iterator   // Code of: https://people.csail.mit.edu/albert/bluez-...

OBaselga by Associate III
  • 1378 Views
  • 0 replies
  • 0 kudos