2021-08-01 11:27 PM
2021-08-04 8:59 AM
The latest is V3.0
https://www.st.com/en/embedded-software/stm32mp1dev.html#overview&secondary=st-get-software
2021-08-02 4:54 AM
Hello KS.2 (Community Member)
Have you tried https://wiki.st.com/stm32mpu/wiki/How_to_read_or_write_peripheral_registers
2021-08-02 5:14 AM
Hi OliverK
yes i followed the same link and installed the devmem2 starter package.
I tried the baudrate command and led command and receieved the error.
dev/mem opened
Error at line 75, file devmem2.c (1) [Operation not permitted]
This is the error message
2021-08-02 8:04 AM
Hi KS.2 (Community Member)
I've just installed devmem2 it via the starter package and tried the command, no issue to be reported.
Are you using the latest starter package image (V3.0.x)?
root@stm32mp1:~# apt-get update
The software package is provided AS IS, and by downloading it, you agree to be
bound to the terms of the software license agreement (SLA).
The detailed content licenses can be found at
https://wiki.st.com/stm32mpu/wiki/OpenSTLinux_licenses.
Get:1 http://packages.openstlinux.st.com/3.0 dunfell InRelease [3458 B]
Get:2 http://packages.openstlinux.st.com/3.0 dunfell/main armhf Packages [1005 ]
Get:3 http://packages.openstlinux.st.com/3.0 dunfell/updates armhf Packages [29]
Get:4 http://packages.openstlinux.st.com/3.0 dunfell/untested armhf Packages [1]
Fetched 2477 kB in 4s (554 kB/s)
Reading package lists... Done
root@stm32mp1:~# apt-get install devmem2
Reading package lists... Done
Building dependency tree... Done
The following NEW packages will be installed:
devmem2
0 upgraded, 1 newly installed, 0 to remove and 0 not upgraded.
Need to get 2984 B of archives.
After this operation, 0 B of additional disk space will be used.
Get:1 http://packages.openstlinux.st.com/3.0 dunfell/untested armhf devmem2 arm]
Fetched 2984 B in 0s (3572 B/s)
The software package is provided AS IS, and by downloading it, you agree to be
bound to the terms of the software license agreement (SLA).
The detailed content licenses can be found at
https://wiki.st.com/stm32mpu/wiki/OpenSTLinux_licenses.
Selecting previously unselected package devmem2.
(Reading database ... 14610 files and directories currently installed.)
Preparing to unpack .../devmem2_1.0-r7_armhf.deb ...
Unpacking devmem2 (1.0-r7) ...
Setting up devmem2 (1.0-r7) ...
root@stm32mp1:~# devmem2 0x4001000C
/dev/mem opened.
Memory mapped at address 0xb6feb000.
Read at address 0x4001000C (0xb6feb00c): 0x0000022C
root@stm32mp1:~#
2021-08-03 1:58 AM
root@stm32mp1:~# apt-get update
The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA).
The detailed content licenses can be found at https://wiki.st.com/stm32mpu/wiki/OpenSTLinux_licenses.
Err:1 http://packages.openstlinux.st.com/2.0 dunfell InRelease
Temporary failure resolving 'packages.openstlinux.st.com'
Reading package lists... Done
W: Failed to fetch http://packages.openstlinux.st.com/2.0/dists/dunfell/InRelease Temporary failure resolving 'packages.openstlinux.st.com'
W: Some index files failed to download. They have been ignored, or old ones used instead.
i am getting this error while trying to update,how to resolve this seems like a dnss issue
2021-08-03 2:06 AM
root@stm32mp1:/etc# cat resolv.conf
# This file is managed by man:systemd-resolved(8). Do not edit.
#
# This is a dynamic resolv.conf file for connecting local clients directly to
# all known uplink DNS servers. This file lists all configured search domains.
#
# Third party programs must not access this file directly, but only through the
# symlink at /etc/resolv.conf. To manage man:resolv.conf(5) in a different way,
# replace this symlink by a static file or a different symlink.
#
# See man:systemd-resolved.service(8) for details about the supported modes of
# operation for /etc/resolv.conf.
nameserver 1.1.1.1
nameserver 8.8.8.8
nameserver 1.0.0.1
# Too many DNS servers configured, the following entries may be ignored.
nameserver 8.8.4.4
nameserver 2606:4700:4700::1111
nameserver 2001:4860:4860::8888
nameserver 2606:4700:4700::1001
nameserver 2001:4860:4860::8844
i think this is the reason as all the entries are being ignored
however i am unable to edit the resolv.conf file
is there any way usual editors are not working(nano,vim,gedit..
)
2021-08-03 5:23 AM
It looks like you are not using the latest openstlinux packages, are you sure you currently use a V3.0 starter image?
In /etc/apt/sources.list.d#, you should point to a debian package V3.0 (not V2.x)
There is vi that come as std to edit. Others need to be installed.
2021-08-03 5:35 AM
The resolv.conf is the issue i guess
nameserver 1.1.1.1
nameserver 8.8.8.8
nameserver 1.0.0.1
# Too many DNS servers configured, the following entries may be ignored.
nameserver 8.8.4.4
nameserver 2606:4700:4700::1111
nameserver 2001:4860:4860::8888
nameserver 2606:4700:4700::1001
nameserver 2001:4860:4860::8844
since all the servers are being ignored the dnss is not working
is there a way to edit the resolve.conf permanently
i tried overwriting using cat but it keeps changing once i reset the board.
2021-08-03 5:42 AM
yea we r using v2.0
2021-08-03 6:26 AM
You can also refer to this article for manual setup: https://wiki.st.com/stm32mpu/wiki/Package_repository_for_OpenSTLinux_distribution#Prequisite
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.