STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! stm32mp157 USB printer support

Hello,​I need use STM32MP157 connect a USB printer. I followed this article(https://community.st.com/s/question/0D53W00000cSjHuSAK/stm32mp157dk2-printer-support?t=1630032775565), and the result is right. but when I use print command like (lp printer_...

xkun.1 by Associate II
  • 2681 Views
  • 3 replies
  • 0 kudos

Resolved! STM32MP1 U-Boot freezes while "Starting Kernel" (stalls on "Waiting for root device" in earlyprink)

I have an STM32MP157D-DK1 board, and I'm trying to build a custom Linux image for it with the Yocto Project. I followed the guide here (https://forum.digikey.com/t/yocto-getting-started-with-the-stm32mp157/14074) to create a core-image-minimal.I’m tr...

Hi, I have created a STM32 project using STM32CubeIDE , Now I need to integrate Cortex-M4 firmware with distribution on yocto.

I copied the STM32CubeIDE project into PATH: openstlinux-5.10-dunfell-mp1-21-03-31/layers/sources/m4projects-stm32mp1/Projects/STM32MP1Added projects path in recipes-extended/m4projects/m4projects-stm32mp1.bbBut i find that file structure for exampl...

Maksh.1 by Associate III
  • 1394 Views
  • 1 replies
  • 1 kudos

Resolved! DMA UserSpace application

Hi all,I am trying to write a linux user-space application where in i am taking data from an external MCU processing it and sending it to another thread. My question here is how can make use of DMA in the user-space to make it more efficient? How can...

NPal.2 by Senior
  • 1778 Views
  • 2 replies
  • 1 kudos