cancel
Showing results for 
Search instead for 
Did you mean: 

Is there a chance to perhaps get a video tutorials, of step-by-step for kernel-configuration-uploading ?

Arnas Celkys
Associate II

I have two codes running (on stm32mp157f-Dk2) successfully one is running on M4+freeRTOS another on A7+Linux, they are intercommunicating via RPMSGx. The problem is that after power-loss or reboot, I want both of my programs starting automatically and not the default UI (GNU desktop screen with icons of examples). Is there a chance to get either step-by-step guide or even better a video executing all the steps to change the kernel and launch customer's code?

4 Build the Linux® kernel source code for the first time:

https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157x-DK2/Develop_on_Arm%C2%AE_Cortex%C2%AE-A7/Modify,_rebuild_and_reload_the_Linux%C2%AE_kernel#Build_the_Linux-C2-AE_kernel_source_code_for_the_first_time

(4.1.2 Remote processor 'auto' boot (not recommended by STMicroelectronics):(

https://wiki.st.com/stm32mpu/wiki/Linux_remoteproc_framework_overview

3.3 Modifying the Linux kernel device tree:

https://wiki.st.com/stm32mpu/wiki/How_to_cross-compile_with_the_Distribution_Package

Because the url guide is a bit unclear it seems to be missing some information.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
PatrickF
ST Employee

Hi,

Except if you need to recompile the kernel, for a simple DT update (e.g. from CubeMX to target), please see https://wiki.st.com/stm32mpu/wiki/How_to_compile_the_device_tree_with_the_Developer_Package

To start M4 FW automatically, I recommend to start from a Linux script executed during startup (there is may ways, depend on your application environment). This is done by simply including the few command lines present in https://wiki.st.com/stm32mpu/wiki/Linux_remoteproc_framework_overview#Remote_processor_boot_through_sysfs

To avoid the launch of the demo, you could for instance adapt the /usr/local/weston-start-at-startup/start_up_demo_launcher.sh file (assuming you still need Weston).

Some video link (not sure they are up to date with latest ecosystem v3)

https://www.youtube.com/c/stmicroelectronics/search?query=stm32mp1

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here

View solution in original post

1 REPLY 1
PatrickF
ST Employee

Hi,

Except if you need to recompile the kernel, for a simple DT update (e.g. from CubeMX to target), please see https://wiki.st.com/stm32mpu/wiki/How_to_compile_the_device_tree_with_the_Developer_Package

To start M4 FW automatically, I recommend to start from a Linux script executed during startup (there is may ways, depend on your application environment). This is done by simply including the few command lines present in https://wiki.st.com/stm32mpu/wiki/Linux_remoteproc_framework_overview#Remote_processor_boot_through_sysfs

To avoid the launch of the demo, you could for instance adapt the /usr/local/weston-start-at-startup/start_up_demo_launcher.sh file (assuming you still need Weston).

Some video link (not sure they are up to date with latest ecosystem v3)

https://www.youtube.com/c/stmicroelectronics/search?query=stm32mp1

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here