STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Regarding STM32mp157A UART in U BOOT

Hi,We are using stm32mp157a processor and we are working on uboot-v2018.11 at Linux side. I have an idea on board-debug-uart_init().Path for board_debug_uart_init().Path :board/st/stm32mp1/board.cIn board-debug-uart_init() .We have only UART_TX infor...

在根�?�ST�??供的tf-a编译阶段,为什么我使用make -f Makefile.sdk TF_A_CONFIG=trusted TFA_DEVICETREE=stm32mp157c-dk2 all这个指令编译的时候会报下�?�这些错误?

在根�?�ST�??供的tf-a编译阶段,为什么我使用make -f Makefile.sdk TF_A_CONFIG=trusted TFA_DEVICETREE=stm32mp157c-dk2 all这个指令编译的时候会报下�?�这些错误?

Ffu.1 by Associate II
  • 7496 Views
  • 7 replies
  • 0 kudos

Resolved! Can someone please help. We are trying to implement a KSZ8041FTL Ethernet PHY using an STM32MP157C. We are not able to connect to the device via MDIO. The device does not respond.

We are trying to implement a KSZ8041FTL in an embedded design. We are using an STM32MP157 device in a SOC provided by Octavo systems (OSD32MP157C-512M-BAA). We have used design resources provided by Microchip and followed examples provided. We have f...

PZak.1 by Associate III
  • 25313 Views
  • 18 replies
  • 0 kudos

ksz8041 bring up

It seems that I have a problem with DMA, but I'm not sure. Would you please take a look at the below screenDts looksI intend to achieve MII with self-generated quartz.Unfortunately, I'm stuck on this "Failed to reset the DMA".

0693W00000FDX7aQAH.png 0693W00000FDX7zQAH.jpg 0693W00000FDX84QAH.jpg
MWoło.2 by Senior III
  • 9896 Views
  • 22 replies
  • 0 kudos

Resolved! I just received STM32MP157F-EV1. On boot, the LCD displays nothing and the onboard ST-Link will not properly enumerate (Windows says "USB Device Not Recognized"). Latest ST-Link driver is installed and working with other kits. Is this a faulty board?

The ST-Link LEDs are very dimly lit when powered...they are much brighter on my STM32MP157F-DK2 board. I suspect some hardware problem with the MPU board. Also, the CPU LEDs do appear to be running (the Linux Blue LED blinks after a while, and with...

DPade.1 by Associate III
  • 2480 Views
  • 3 replies
  • 0 kudos