2021-06-14 1:58 AM
a tsv file with
#Opt id Name Type IP Offset Binary
- 0x01 fsbl Binary none 0x00000000 u-boot-spl.stm32I got different error messages:
sending a dfu end of download request
DFU status = 0
DFU State = 7
DFU status = 14
DFU State = 10
an error occured after sending a dfu end of download request
Status: errUNKNOWN, State: dfuERROR
Error: Start operation failed at partition 0x01
Error: TSV flashing service failed
Warning: Connection to device 0x500 is lostFile download complete
Time elapsed during download operation: 00:00:02.924
RUNNING Program ...
PartID: :0x01
Error: Start operation failed at partition 0x01
Error: TSV flashing service failed
Warning: Connection to device 0x500 is lostFile download complete
Time elapsed during download operation: 00:00:02.863
RUNNING Program ...
Address: : 0x1
Error: an error occured while uploading data from the virtual partition 0xF1
Start operation achieved successfully
2021-06-14 2:03 AM
Hi @Lmoio.1 ,
Did you already successfully boot the same custom board with Trusted boot chain ?
How did you manage Device Tree customization for you board ?
Can you share Console output during CubeProg execution ?
Thx,
Olivier
2021-06-14 2:10 AM
No, I get the same error at partition 1.
For the moment we are using the Device Tree from the stm32mp157c-ev1.
With trusted boot chain, there is nothing in the console.
With basic boot chain, there is:
U-Boot SPL 2020.10-stm32mp-r1-gbde7c9b2f1 (Jun 14 2021 - 10:00:44 +0200)
Model: STMicroelectronics STM32MP157C eval daughter on eval mother
RAM: DDR3-DDR3L 32bits 533000kHz
0:DDR_RESET
2021-06-14 3:13 AM
Hi @Lmoio.1 ,
Strange you don't have even a single trace in Trusted boot mode.
You are using stm32mp157c-ev1 DT. I assume then your design is similar or very close ?
Any difference ?
Did you have same DDR reference and configuration ?
I presume you are trying to use Serial USB boot ?
Did you follow carefully recommendation in AN5031 Getting started with STM32MP151, STM32MP153 and STM32MP157 line hardware development for OTG_HS_DP/DM pins and for boot pins ?
Olivier