STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Hello, i'd like to use u-boot command sspi to send commands to a spi device with a custom protocol (not a memory). However I see that the command tries to read an ID as it is talking to a flash nor : unrecognized JEDEC id bytes: 00, 00, 00.

Looking at the code, i see file sf_probe.c with .id      = UCLASS_SPI_FLASH, that performs the id reading. How can i use stm32_spi.c with .id         = UCLASS_SPI, driver instead? and send "raw" spi data?

Lmoio.1 by Senior
  • 9053 Views
  • 8 replies
  • 0 kudos

Resolved! Hello, I've exported our custom root filesystem from a running board with the following command: dd if=/dev/mmcblk1p4 of=/usr/local/rtfs.ext4 bs=1M conv=fdatasync

I noticed that after I flash the ST starter package root filesystem, at first boot there is a check on bad blocks and a resize of the partitions, while when I flash the exported root filesystem, there is no checks and some partitions are not resized ...

Lmoio.1 by Senior
  • 3840 Views
  • 5 replies
  • 0 kudos

I'm not using USB nor ADC/DAC on the STM32MP157A. Can I tie VDDA, OTG_VBUS, AND VDD3V3_USBxS to circuit ground (VSS)?

If I'm interpreting Table 13 correctly (datasheet p 128), VDDA can be set to 0 volts provided VREF is not used. Similarly power pins related to USB can also be set to 0 volts. Looking in the datasheet p29,I just need to star-connect VDD_ANA, VDD_PLL...

JCond.1 by Associate II
  • 3786 Views
  • 3 replies
  • 0 kudos

Resolved! Out of order STM32MP157CAC. PANIC at PC : 0x2fff2d17 Exception mode=0x00000016 at: 0x2fff2d17

Hello.I developed my own board based on A-DK1 board using STM32MP157CAC and MicroSD, PMIC, Ethernet and DDR periphery. When I connect my plate to the usb with sd-card (st-link 2.1) I always receive the message:PANIC at PC : 0x2fff2d17Exception mode=0...

DFomi.1 by Associate II
  • 4169 Views
  • 2 replies
  • 0 kudos

Resolved! The question about STM32MP157CAC3 supply

Hello. I have used the STM32MP157A-DK1 this year and I have learned to work with it. Now I develop my own PCB with STM32MP157CAC3. There is a 12-V external power supplier in it. I do't use USB Type-C. Can I do like this? I care about pins USB_PWR_CC1...

DFomi.1 by Associate II
  • 3100 Views
  • 5 replies
  • 0 kudos