STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to enable SPI1 on the M4 side?

I am describing my approach as below:What we did:1) We are using the STM32MP157F-EV1 board (No other board is connected for this exercise, lines are open!)2) We are using OpenSTLinux(kernel:5.4) and we are using the firmware which was suggested under...

Reduce image size with Yocto

Hello, I've got a board with an STM32 MP CPU and I have to reduce the size of the final image to leave enough space on the NAND memory for a dual rootfs setup. The idea is to remove the alsa layer because I don't need the audio part. I tried to add t...

LLorr.1 by Associate
  • 2278 Views
  • 2 replies
  • 0 kudos

ADC Multiple channel interrupt routine

Hello,I have 7 ADC channel , and its configue as interrupt. But the interrupt each is get generated for different condition how I can check the which ADC channel interrupt is get generated which I have to use the function for distinguish the ADC chan...

MDeva.1 by Associate II
  • 1347 Views
  • 1 replies
  • 0 kudos

Resolved! mozjs_60.9.0.bb:do_compile failed with exit code '1 - Cant Compile Distribution Package (SOLVED)

I've followed all the steps from:https://wiki.st.com/stm32mpu/wiki/STM32MP15_Discovery_kits_-_Starter_Packagehttps://wiki.st.com/stm32mpu/wiki/PC_prerequisiteshttps://wiki.st.com/stm32mpu/wiki/STM32MP1_Distribution_PackageCreating openstlinux-5.10-du...

0693W00000BcokoQAB.png 0693W00000BcolgQAB.png