STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32MP1 repo sync error while downloading distrubution package layers. error: garbage at end of loose object '543a1d1527d04f297b90ec25658f8dc71f3d0782'

I was trying to install OpenSTLinux distribution. I am using ubuntu 20.04 for my host machine. Firstly I init repo with this command:repo init -u <LINK FOR GIT ST OE MANIFEST > -b refs/tags/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15 then when...

Gencay by Associate III
  • 2155 Views
  • 6 replies
  • 0 kudos

Resolved! How to read otp register in linux?

I need to store a password for encryption in otp registers. I configured device tree in tfa:&bsec{ status = "okay"; secure-status = "okay"; enc_pass: enc_pass@0x170 { reg = <0x170 0x10>; st,non-secure-otp; };};&nvmem_layout {    nvmem-cells = <&enc_p...

MJerm.1 by Associate II
  • 3142 Views
  • 3 replies
  • 0 kudos

Resolved! Access Tampers and BckSRAM from M4.

Hello,Is there a way to access the Tamper or backup registers or the backup sram from the MCU? Or is it physically imposible to do so?Edit:I am still looking for an answer, I just saw in the RCC registers that I can enable BKPSRAM bits to:enable the ...

AGamb.4 by Associate III
  • 3129 Views
  • 4 replies
  • 0 kudos