STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Error during repo init -u https://github.com/STMicroelectronics/oe-manifest.git -b refs/tags/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15

Hello,I try to install the distribution package usingrepo init -u https://github.com/STMicroelectronics/oe-manifest.git -b refs/tags/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15as described in the wiki, before that made sure to install all packages...

SFuch.1 by Associate III
  • 1878 Views
  • 1 replies
  • 0 kudos

Resolved! Secure boot documantation

Is there a walk-through or example of how to setup secure boot using a custom device tree?As a side note, the following page returns "Permission Error", is that expected behaviour?https://wiki.st.com/stm32mpu/wiki/STM32MP15_secure_boot

0693W00000QNd3iQAD.png

Resolved! File handling functions (fread, fwrite, getc, fseek, etc.) do not work in the STM32MP15x Cortex A7 core. Why is that and is there a solution for it?

Hello,When I tried using fseek and getc functions for my project the MP1 failed to execute their code. The execution stops at lines that contain __IO_acquire_lock(fp) and __IO_need_lock(fp) macros and then terminates in the fseek and getc functions r...

Yamir.1 by Associate II
  • 2169 Views
  • 1 replies
  • 0 kudos

Resolved! When I use bitbake PermissionError: [Errno 13] Permission denied: '/home/dev' error occurs

I've changed the ownership of the /usr/lib/python3.8 file from root to <myname> but did not solved the problem. Here is the whole error:ERROR: Command execution failed: Traceback (most recent call last): File "/home/gencay/STM32MPU_workspace/openstli...

Gencay by Associate III
  • 6070 Views
  • 4 replies
  • 0 kudos

Resolved! Hi: I'm using st-image-weston-openstlinux-weston-stm32mp1.ext4. The USB mouse works, but the touch screen doesn't respond.

Using hexdump /dev/input/event1, you can see the data changes. when I use ts_ test command, "open fbdevice: no such file or directory" will appear. Please help me, I really don't know how to configure it.I am sure that the touch screen monitoring is ...

zxiao.4 by Associate III
  • 6066 Views
  • 7 replies
  • 1 kudos

Resolved! How to configure PTP PPS out?

Hi!   I am trying to enable PTP on STM32F157 DK2 evaluation board.   From my understanding, pps_available should return 1, (if configured correctly).   root@stm32mp1:~# cat /sys/class/ptp/ptp0/pps_available 0 I added "linuxptp" to the image: IMAGE_I...

GLaure by Senior
  • 11091 Views
  • 10 replies
  • 0 kudos

STM32MP157F-DK, Run the SDK installation Error and Try to run python with Linux or flash it

I'd try to follow a step of Installing the SDK in Ubuntu (which is on Raspberry pi 4 Model B 4GB using 26GB SD card)in step 4 Run the SDK installation script I get an Error Error: incompatible SDK installer! your host is aarch64 and this SDK was buil...

PMeth.3 by Associate
  • 1173 Views
  • 1 replies
  • 0 kudos

Contact for academia

Hi there. I'm a professor of computer science at a university in Germany. Our main focus is cyber security. I'm currently looking into exploring options with STM for teaching various security mechanisms and, in particular, interested in using the STM...

monnem by Associate
  • 1454 Views
  • 2 replies
  • 0 kudos