In the en.STM32Cube_FW_MP1_V1-5-0.zip file, there are several example projects designed for the STM32MP157C-DK2. I know that there are differences with the clocks, so it would be nice to have a set of instructions indicating which clocks in the CubeM...
I switch power supplies and now I am able to Flash the SD Card.Good = Ultranet CX65UC002 Ultron GaN 65W Type-C PD ChargerBad = CUI Inc. SWC15-S5-NB Wall Mount AC Adapter 15W 5V 3AThank you
Attached is the output of the console (TeraTerm), and the log from the Cube programmer.I am using the 157a-dk1 TSV file. My system does the same thing when using the command line.I have even tried to 'Disabled' the Windows 10 Power Option to selecti...