cancel
Showing results for 
Search instead for 
Did you mean: 

STM32MP1 ISO7816 interface

Dowlers
Associate

Hi

I see the STM32MP1 has an ISO7816 interface, is there Linux device driver support for the ISO7816 interface. Or is there any documentation on how I might enable support for this.

Thank you,

Eoin

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
OlivierK
ST Employee

Hi Dowlers (Community Member)

Yes there is indeed an ISO7816 interface on STM32MP1, but we don't have a Linux driver available yet.

But your are not the only one to ask, the subject in the pipe internally to be included in a future OpenSTLinux release and/or may rely on partners to implement it.

Sorry, I don't have any documentation to provide for now.

Regards,

Olivier


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
OK thank you Oliver

Any news about the ISO7816 interface on STM32MP1?