cancel
Showing results for 
Search instead for 
Did you mean: 

stm32mp157dk2 Ethernet irq poll

AVazquez
Associate III

Hi!

I have been reviewing the kernel log for the DK2 Kit, and I have noticed that the Ethernet configuration is in polling mode.

 

[   37.074899] stm32-dwmac 5800a000.ethernet eth0: PHY [stmmac-0:00] driver [RTL8211F Gigabit Ethernet] (irq=POLL)

 

Is there a specific reason for the decision to have it in polling mode?

Upon examining the schematic, I can see that the interrupt signal is on PA6(ETH_MDINT).

I understand that the configuration for the interruption should be:

 

interrupt-parent = <&gpioa>;
interrupts = <6 IRQ_TYPE_EDGE_FALLING>;

 

 

 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
PatrickF
ST Employee

Hi @AVazquez ,

I assume this is very similar of this post: https://community.st.com/t5/stm32-mpus-products/alternate-function-eth1-phy-intn-from-stm32mp15c/m-p/595868

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here

View solution in original post

1 REPLY 1
PatrickF
ST Employee

Hi @AVazquez ,

I assume this is very similar of this post: https://community.st.com/t5/stm32-mpus-products/alternate-function-eth1-phy-intn-from-stm32mp15c/m-p/595868

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here