STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32MP1 FMC address pins

Hello!I have a MP1 board (STM32MP157), and i was wondering if one can have control over which individual pins are used when it comes to FMC. I want to use FMC for PSRAM, 8-bit data mode, but the pin that corresponds to FMC_A2 is already in use (PF2),...

Resolved! eMMC flashing with GPT partition table

Hi ST Community,I am trying to flash a eMMC with STM32CubeProgrammer, in a STM32MP157F custom board. I am using a GPT partition file and a img.I can see the system is creating partitions and flashing, but the structure is wrong for eMMC, so it does n...

Flyback_0-1698484449426.png Flyback_1-1698484522541.png
Flyback by Associate II
  • 5707 Views
  • 2 replies
  • 0 kudos

STM32MP1 Switch to Production Boot

I have a board where a secondary CPU can select the STM32MP1's boot mode.  On initial boot, the MP1 boots from NOR flash.  I can then send a command to the secondary CPU which switches the MP1's BOOTx pins to enable engineering boot and resets the MP...

DPade.1 by Associate III
  • 4600 Views
  • 5 replies
  • 0 kudos

STM32MP157d USART1

Hi,What am I doing wrong that USART1 returns -2 during the probekernel.dts -> PINS   usart1_pins_mx: usart1_mx-0 { pins1 { pinmux = <STM32_PINMUX('A', 9, AF7)>, /* USART1_TX */ <STM32_PINMUX('A', 12, AF7)>; /* USART1_RTS */ bias-disable...

Resolved! LPLV-Stop

Please tell me how to set the wake-up button (PA0:PWR_WKUP) as a return factor from LPLV-Stop mode and set STM32MP157f-EV1 to LPLV-Stop mode.

kiichi by Associate III
  • 5333 Views
  • 2 replies
  • 1 kudos