cancel
Showing results for 
Search instead for 
Did you mean: 

OPTEE Core data-abort problem.

Macdog
Associate III

We recently udated from OpenSTLinux v2.1 to v4.1. The boot chain is solid, but occasionally we are getting TEE aborts (trace listed below). I am not sure exactly how to debug this, any help would be appreciated.

E/TC:1

E/TC:1  Core data-abort at address 0x2fff8805 (translation fault)

E/TC:1   fsr 0x00000207 ttbr0 0x2ffd8020 ttbr1 0x00000000 cidr 0x0

E/TC:1   cpu #1         cpsr 0x000001f3

E/TC:1   r0 0x2fff8805     r4 0x2ffda889   r8 0x2ffda889  r12 0xffffffe0

E/TC:1   r1 0x2ffcda91     r5 0x000000f7   r9 0x00000000   sp 0x2ffda788

E/TC:1   r2 0x2fff8805     r6 0x00000000  r10 0x2fff8805   lr 0x2ffcb297

E/TC:1   r3 0x2fff8806     r7 0x2ffda870  r11 0xffffffff   pc 0x2ffcac80

E/TC:1  TEE load address @ 0x2ffc0000

E/TC:1  Panic 'abort outside thread context' at ?:0

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Macdog
Associate III

Just in case anyone is interested, our problem was a simple device tree oversight. We had neglected to inlude the reserved memory for optee in our kernel device tree when updating from TF-A boot chain to OP-TEE boot chain:

```

        optee@de000000 {

            reg = <0xde000000 0x2000000>;

            no-map;

        };

```

View solution in original post

3 REPLIES 3
Kevin HUBER
ST Employee

Hello @Community member​ ,

please can you share the complete boot log?

Best Regards,

Kevin

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
NEW ! Sidekick STM32 AI agent, see here
Macdog
Associate III

Thanks, Kevin, for responding!

Some more context: we are building our own distribution using buildroot. On top of that we are running Nerves (Erlang BEAM / Elixir main application). The exception reliable presents when we do a firmware update through our web interface (Phoenix/Cowboy server). The firmware file uploads successfully (written to a read/write partition formatted as F2FS), and aborts when attempting to overwrite the GPT partition table. The partition table overwrite is how Nerves manages firmware A/B with fallback.

Attached is the boot log up to and including the abort.

Macdog
Associate III

Just in case anyone is interested, our problem was a simple device tree oversight. We had neglected to inlude the reserved memory for optee in our kernel device tree when updating from TF-A boot chain to OP-TEE boot chain:

```

        optee@de000000 {

            reg = <0xde000000 0x2000000>;

            no-map;

        };

```