cancel
Showing results for 
Search instead for 
Did you mean: 

MIPI display blank after enabling uart8

Rc.1
Associate II

I'm using a custom stm32mp157a board with a DSI display.

If I enable uart8 using pins J8 (UART8_TX) and J9 (UART8_RX) the display driver (panel-sitronix-st7701.c) doesnt load properly and the display stays blank.

uart8 does work properly. If I disable uart8 the display works again.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Kevin HUBER
ST Employee

Hello @Rc.1​ ,

Please can you share your complete boot log and your dtb file used.

Does the problem occurs only in Linux or directly from the boot?

Best Regards,

Kevin

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
NEW ! Sidekick STM32 AI agent, see here