STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB Gadget does not recognize disconnect

Hello,I'm kind of stuck with my STM32MP157C custom board. In general, everything works fine except for the USB. I'm using the new Ecosystem 5 and using the USB OTG with the NCM Ethernet gadget. My USB has no ID pin wired and is in peripheral mode all...

JSala.3 by Associate II
  • 2958 Views
  • 1 replies
  • 0 kudos

Resolved! Disable JTAG

Good morning,I would like to know if I can disable the JTAG in the STM32MP1. Once my project is finished I do not want this interface to be active. Is there a way to disable the JTAG/SWD interface with registers/fuses/OTP?Kind regards,Andrés

AGamb.4 by Associate III
  • 3396 Views
  • 2 replies
  • 0 kudos

USART is really working in stmp157 ?

Hi All,i am using stmp157 customize board, with linux yocto build system, and using USART1 configure as a hardware flow control RS 232, and RTO interrupt. and what i found is that CTSIF is not toggling and the proper status are not getting update on ...

Vipul by Associate II
  • 2224 Views
  • 2 replies
  • 0 kudos

Resolved! stm32mp135 yocto build process

 i have download prebuild image en.flash-stm32mp1-openstlinux-6-1-yocto-mickledore-mp1-v23-06-21.tar.gzit working fine on my stm32mp135f-dk EVK. i want to add docker in it so need the build process of yocto image.Kindly guide me how to do it.