User Activity

Hello,I am using STM32F769I - Discovery board. I want to roate the display by 90 degrees clockwise. Regards,Nitesh
Hi,I have written a cpp program with two threads, one thread for uart serial communication and other thread to control the GPIOsi have compiled it, and i got a binaryButWhen i transfered it to the board i get the error ./fw_dali_controller: line 1: s...
Hi,I want to configure the LED7 of stm32mp157f-dk2, in arc/arm/boot/dts folder there are stm32mp157f-dk2.dts and stm32mp157f-dk2.dtb file, I cannot edit .dts file since it appears as an audio file and not the text file.so I edited the stm32mp15xx-dxx...
Hi I am using STM32mp157-DK2 for the first time.I am trying out the section Modify, rebuild and reload the linux kernel which is described in following linkhttps://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157x-DK2/Develop_on_A...
Kudos given to