2024-05-15 06:38 AM - edited 2024-05-15 06:58 AM
Hi All,
I have been a little confused about my code and would appreciate some help greatly...
I have a basic program where I would like to read the ADC values from a sensor, and transmit them via UART for later signal processing and whatnot.
The structure is simple, and when I tested out reading the values from the ADC, as well as sending strings via UART - they both work perfectly fine. But now when I merge the two, the UART does not work anymore... I do not see anything in my serial monitor (Putty)
I feel like I am missing something big, but cannot find it. I would appreciate it if someone pointed me in the right direction 🙂
in my main, I have:
uint32_t value[2]; // start adc in DMA mode
int isSent = 1;
uint8_t tx_buffer[] = "Welcome to BinaryUpdates!\n\r";
int main(void)
{
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_DMA_Init();
MX_ADC1_Init();
MX_TIM3_Init();
MX_TIM4_Init();
MX_TIM2_Init();
MX_USART6_UART_Init();
HAL_ADC_Start_DMA(&hadc1, value, 2);
while (1)
{
if (isSent == 1)
{
HAL_UART_Transmit_DMA(&huart6, tx_buffer, 27);
// HAL_UART_Transmit_DMA(&huart6, value[0], sizeof(value[0]));
isSent = 0;
}
HAL_Delay(1000);
}
}
void HAL_UART_TxCpltCallback(UART_HandleTypeDef *huart)
{
isSent = 1;
}
2024-05-15 07:55 AM
@ponuliukas wrote:It works alone, but If I start the ADC DMA, it doesn't work.
What if you use the ADC without DMA ?
2024-05-16 02:56 AM
I will try that in a second and will let you know how it goes.
What I have found out is that if I toggle an LED every 500ms, it works perfectly alone, but then if I uncomment the "HAL_ADC_Start_DMA(&hadc1, value, 2);", the LED gets stuck on always ON.
2024-05-16 03:17 AM
@ponuliukas wrote:What I have found out is that if I toggle an LED every 500ms, it works perfectly alone, but then if I uncomment the "HAL_ADC_Start_DMA(&hadc1, value, 2);", the LED gets stuck on always ON.
So it's not just the UART which stops working after you call HAL_ADC_Start_DMA - even a simple LED blink stops working?
Have you used the debugger to check if HAL_ADC_Start_DMA is returning at all ?
Or are you getting stuck in a Hard Fault or other Error Handler?
If HAL_ADC_Start_DMA does return, what result code does it give? Again, see:
2024-05-16 03:47 AM
If I run just the HAL_ADC_Start_DMA , then when I press on my pressure sensor - the values are visible in the live expressions - they go from 0 to 2555, which is a value I expect.
2024-05-16 03:49 AM
So where does the toggling LED come into that?
2024-05-16 03:51 AM
I just toggle it in the main while loop (RGB LED, and I just toggle the red channel) to see if the program would still function correctly when I read the ADC with my sensor values.
while (1)
{
int del = 500;
htim4.Instance->CCR1 = 255;
HAL_Delay(del);
htim4.Instance->CCR1 = 0;
HAL_Delay(del);
}
2024-05-20 02:44 AM
Coming back with a little breakthrough - but not sure how ideal this situation is.
If I change the DMA for ADC from "circular" to "normal", and put the two in the main while loop, then I manage to read the ADC values and send them via UART.
while (1)
{
HAL_ADC_Start_DMA(&hadc1, value, 2);
raw = value[0];
sprintf(buffer, "%u\n\r", raw); \\ char buffer[7]
HAL_UART_Transmit(&huart6, (uint8_t*)buffer, strlen(buffer), HAL_MAX_DELAY);
}
I was wondering whether in your opinion this is a bad way to do this. Should I use interrupts instead, or if it is not broken, then don't fix it?