2022-03-08 9:50 PM
hey there
I have a STM32f030C8t6 which I wish to read 2 Analog values by it. I use ADC DMA for this. but as soon as I use command
HAL_ADC_Start_DMA(&hadc,(uint32_t *)ADC_SEN,2); //Starting ADC1
I can see my ADC pins' volt are as high as 3.5volts!
why is that?
2022-03-08 9:59 PM
How do you measure these 3.5V ?
Anything connected to the GPIOs?
Configured as ADC inputs?
Anyway, it it is an open input, a lot of things can occur, and measurements of the GPIO with a DMM might not make sense (leakage currents, rectified high frequencies, ...).
So check your configuration and start connecting low voltages, for example take a 10k / 10k voltage divider to measure half VCC. For other voltages make sure these are within the limits, better always use a serial resistor (+ small cap for filtering) between signal and ADC input. I don't know about the ADC's input impedance, check the datasheet if you can use 10k or should use a lower value, but I wouldn't start below 1k.
2022-03-08 10:07 PM
I measure this 3.5V using a multimeter.
my ADC pins are now open, meaning nothing is connected to them.
I just generated the code using my configuration in CubeMx, but I did not add any code just to make sure my configuration itself is OK. then I built it in Keil and Loaded it to my board. it was OK. but as soon as I ran
HAL_ADC_Start_DMA(&hadc,(uint32_t *)ADC_SEN,2); //Starting ADC1
piece of code, my ADC values became 3.5V!
2022-03-09 12:22 AM
DMM = Digital MultiMeter, might get you strange results.
So try what I mentioned above, don't leave inputs open, but start with just reading single ADC values, for the beginning without DMA - except you are perfectly sure how to handle it and can access the ADC results.
2022-03-09 12:54 AM
I did exactly as you said: I used a 10K/1K divider and connected it to a 20V source to get 0~2V as ADC input, and the result is unexpected:
the ADC count that I get is always higher than expected! I repeated the test for 11value within above range, and in every test the count was around +1300 higher than expected! this much count for a 12bit MCU is like +1V is given to ADC. I'm confused!
Can you help?
2022-03-09 2:35 AM
Try longer sampling time - 10k/1k divider may represent a relatively high input impedance.
Also make sure you don't have the pin's pullup switched on - read out the respective GPIO_PUPDR content and check.
JW
2022-03-09 3:18 AM
Dear @Community member
where can I find the GPIO_PUPDR content you mentioned?
2022-03-09 4:27 AM
GPIOx_PUPDR are part of the GPIO registers, check the reference manual.
10k / 1k divider and 1V above what it should be sounds like an active internal pull-up.
Depending on your needed bandwidth you could put a small x pF cap in parallel to the 1k.
2022-03-09 5:42 AM
If a pin is higher than VDD, it must be being driven externally through some channel. There are no charge pumps in the MCU which generate higher voltage.
2022-03-09 8:53 PM
seems so logical, but this ADC pin is not attached to anything, even in PCB itself. it's just a track.
anyways, I commented the ADC DMA start in above, and tried to read ADC values by polling. now I doesn't read anything! or reads some gibberish! though when I measure the volt on ADC pin, the volt is delivered right and no fluctualtions... any ideas?