2022-03-09 8:57 AM
// in 1/32768 parts of second, 1 hour (3600*32768) max.
uint32_t cRTC::getCurrentTime32768(){
volatile uint32_t time = 0;
volatile uint16_t takenTime = 0;
volatile uint16_t takenSSR;
volatile uint16_t dummy;
//reading either RTC_SSR or RTC_TR locks the values in the higher-order calendar shadow registers
// until RTC_DR is read! Locking ensure consistency of readden data.
awaitShadowRegUpdate();
takenTime = (uint16_t)RTC->TR;
awaitShadowRegUpdate();
takenSSR = (uint16_t)RTC->SSR;
awaitShadowRegUpdate();
dummy = (uint16_t)RTC->DR;
time = ( ( (takenTime & 0xF0) >> 4 ) * 10 ) + (takenTime & 0xF); // seconds
time += 60 * ( ( ( (takenTime & 0xF000) >> 12 ) * 10 ) + ( (takenTime & 0xF00) >> 8 ) ); // minutes
time = (time*32768) + (32767 - takenSSR);
return time;
}uint32_t cRTC::spentTime32768(uint32_t* startTime){ // with update startTime automatically
volatile uint32_t spent = 0;
volatile uint32_t currentTime = cRTC::getCurrentTime32768();
if(currentTime >= *startTime){
spent = currentTime - *startTime;
} else {
spent = currentTime + ((3600*32768) - *startTime);
}
*startTime = currentTime;
return spent;
}extern "C" void EXTI2_3_IRQHandler(void){
if(READ_BIT(EXTI->RTSR, EXTI_RTSR_TR2)) {// catched rising edge
EXTI->RTSR &= ~EXTI_RTSR_TR2; // Disable rising Trigger
EXTI->FTSR |= EXTI_FTSR_TR2; // Enable falling Trigger
motorStartTime = cRTC::getCurrentTime32768();
motorIsON = true;
}
else {
EXTI->FTSR &= ~EXTI_FTSR_TR2; // Disable falling Trigger
EXTI->RTSR |= EXTI_RTSR_TR2; // Enable rising Trigger
int32_t lastMotorSec = cRTC::spentTime32768(motorStartTime);
motorIsON = false;
}
EXTI->PR |= EXTI_PR_PR2; // Clear Pending Interrupt Flag by writing 1 (PA2)
}
2022-03-09 11:28 AM
Read each value twice or more until they are all the same on consecutive readings to ensure consistent results.
What does awaitShadowRegUpdate do here?
2022-03-09 11:46 AM
Some complete, stand-alone, compilable code, with dumps of the registers, and final computations would go a long way to getting anyone interested in this.
2022-03-10 6:51 AM
Thank You TDK, now I know that shadow registers can be updated unconsistently. Now I use BYPSHAD=1 and read twice each register and compare each, up to 10 times to get equal content. Now I testing my code.