2023-10-02 03:04 AM - edited 2023-10-02 06:29 AM
Dear MCSDK users, MCSDK version 6.2 is now available: Download It here.
Here are the main changes for this version:
Hardware Compatibility :
Motor Control Features:
Tools:
We also introduced new boards like: EVLSPIN32G4-ACT, EVSPIN32G4-DUAL, NUCLEO-C031C6, NUCLEO-H563ZI, NUCLEO-H503RB, B-G473E-ZEST1S-B, STEVAL-LVLP01
The boards here below, already supported in MCSDK 5.4.8, are now supported in MCSDK 6.2.0: STEVAL-IHM039V1, STEVAL-IHM045V1, STEVAL-CTM009V1, STEVAL-IHM042V1, STM32L476G-EVAL, STM32F769I-EVAL
Do not hesitate to respond under this post to give us your opinion about this new version.
Best regards
2023-10-11 11:10 PM
Hi,
I have installed MC SDK 6.2.0. This is the first time looking at the new version of MC SDK. I have extensive experience with custom commercial solutions using 5.4.x-FUL versions.
I would like to create a custom solution, but when I select "New Project" I only see options for creating projects with pre-defined eval boards.
Can you direct me to documentation for creating projects based on custom hardware?
Thanks,
Matt
2023-10-12 01:00 AM
Thank you for your interest in MCSDK 6.2. To create a custom board, you can use the Boards Manager. To launch it, open the Workbench then Tools -> Boards manager. The documentation for the use of this tool is still being validated and should arrive very soon. You can take inspiration from the descriptions of other boards in the meantime.
Best regards
2023-10-12 08:20 AM
Hello, are there plans to support the STEVAL-ESC001V1 board soon. If so, do you know when? I also would be interested in any additional information around creating custom boards using the boards manager.
2023-10-12 02:51 PM
Thank you very much.
Are there any plans to make it interactive, like the previous version?
2023-11-08 01:02 PM - edited 2023-11-08 07:01 PM
2024-01-10 05:08 AM
Can't move to 6.2 yet because I cant adjust the current sensing feedback gain as per my custom board.
Still with 5.Y.2
2024-01-10 06:09 AM
Hello @Muthanna,
If you started from a ST board, then just clone your board in the Board manager tool and change the gain parameters.
Regards,
Cedric
2024-01-11 12:09 AM
Thank you Cedric, The Board Manager was a bit confusing at first, figured it out. Going to make the transition from 5.Y.2 to 6.2.1
Fingers Crossed,
Muthanna