STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1740 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4888 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9585 Views
  • 5 replies
  • 3 kudos

Resolved! HSO Requirement for P-NUCLEO-IHM03 kit

Hi everyone,I am trying to activate HSO option for sensorless control which as much as I know this feature is to start motor without moving, but I cant activate HSO option with these option in attached.I cant find the problem. Thanks in advance.

Zek_De_0-1734882480515.png Zek_De_1-1734882494078.png Zek_De_2-1734882505570.png Zek_De_3-1734882528461.png
Zek_De by Senior
  • 2223 Views
  • 3 replies
  • 0 kudos

Resolved! Feature request: spi encoder

It would be very useful to be able to use an external encoder using any serial protocol.I'm working with a RLS AksIM-2 with SPI, and I don't see an easy way to integrate this encoders with the code generated by the MC Workbench.As at the moment the o...

DAlvarez by Associate II
  • 2336 Views
  • 2 replies
  • 3 kudos

Resolved! control of bldc motor

hello sir/madamI want to control the bldc motor using field oriented control, and soft start the bldc motor. Which stm32 controller and driver should I need to  use, is there any library or sample files available. Please do help me.Thank you !

ses by Associate
  • 2051 Views
  • 1 replies
  • 1 kudos

Resolved! MCSDK, B-G473E with LVLP01 DAC error

Hi,want to use two DAC Channels with MCSDK but I get errors. I can't get any further with the error message.Control Board B-G473E-ZEST1SPower Board STEVAL-LVLP01Speed Sensor Mode:HSO DAC DebugDAC1_OUT1 (PA4)DAC1_OUT2 (PA5)[VERSION]: Version of MCSDK ...

L6480HTR Current problem

We are operating the motor with the Run command “Run(DIR, SPD)” to rotate it at a constant speed. However, when the speed (SPD) is varied and then returned to the same SPD, we observe a significant increase in current.We send the Run command to the d...

TOAMUSEN by Associate
  • 688 Views
  • 0 replies
  • 0 kudos

Torque mode speed limiter

Hello everyone,How can I set a speed limiter when I use the motor in Torque Mode(FOC)?. I am getting an oscillation.I am using St motor control workbench.In addition, motor in speed mode , when I apply a less speed then I am getting the motor in zero...

Zek_De by Senior
  • 951 Views
  • 0 replies
  • 0 kudos

Resolved! Hardware design file

Hi,I am looking for hardware reference design source files for STEVAL-ESC002V1 board.Is it available to speed up the design activity?Thank you for your kind attention and immediate response Sincerely,Raj 

SPI communication of L6482

Hello, I encountered some issues while using SPI to control L6482:1. My read/write SPI logic seems to have failed, unable to read/write normally. Is this a problem with my SPI timing?This is the timing sequence for me to retrieve the status register....

lcc1111_2-1735090518149.png lcc1111_3-1735090550487.png
lcc1111 by Associate
  • 573 Views
  • 0 replies
  • 0 kudos

Dead Time between different channels

I want to configure dead time between different channels but I get the output as in the picture.Below is the PWM function I created for the BLDC motor and algorithm for each phase of BLDC motor. What could be the problem?  void BLDC_SetPhase(uint8_t ...

BLDC_logic.png PWM.jpg