cancel
Showing results for 
Search instead for 
Did you mean: 

ACIM support - which version to use?

lamare
Associate III

On the wiki page:

https://wiki.st.com/stm32mcu/wiki/STM32MotorControl:SDK_AC_induction_motor 

It says:

""This article applies to the 5.Y.* versions series of the X-CUBE-MCSDK. ACIM motors are not supported in older versions of the X-CUBE-MCSDK (v5.4.* and before). They are not supported yet in X-CUBE-MCSDK versions 6.*."

 

However, the latest v5 version I can download is 5.4.8.

 

So, it appears that I would need to use version 6 to compile the examples, while full support comes later?

 

 

 

 

 

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
GMA
ST Employee

Hello @lamare,
Wiki page isn’t up to date (thank you for the report).
Two ACIM examples are available on the latest X-CUBE-MCSDK-6 workbench available here.

GMA_1-1741279630618.png

Loading ACIM example of Motor Control workbench, it’s possible to change parameters and generate a project.

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA

View solution in original post

1 REPLY 1
GMA
ST Employee

Hello @lamare,
Wiki page isn’t up to date (thank you for the report).
Two ACIM examples are available on the latest X-CUBE-MCSDK-6 workbench available here.

GMA_1-1741279630618.png

Loading ACIM example of Motor Control workbench, it’s possible to change parameters and generate a project.

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA