2025-02-05 7:24 PM
[VERSION]: MCWB v6.3.2
[TOOL]: STM32CubeMX v6.13.0, STM32CubeIDE v1.11.5
[BOARD]: STEVAL-PTOOL1V1
[PROJECT]: STEVAL-PTOOL1V1_6S_SL
I've been trying to get this board working with a small BLDC motor but the keeps shutting off the motor output when the speed is brought up a bit. I tried increasing the current limit in the code (I believe although I'm not certain I'm effectively doing that).
I want to see if I can connect a serial port and see messages or use Motor Pilot or Motor Profiler. The documentation for this board doesn't show a UART port mapped to the external pins. Can it be done?
Solved! Go to Solution.
2025-02-11 5:24 AM
Hello @Angelo Quattrociocchi,
According to stspin32f0b datasheet, USART serial interface is available via PB6 and PB7.
These pins are available on STEVAL-PTOOL1V1, J3 connector, pin15/17, refer to board schematic.
2025-02-11 5:24 AM
Hello @Angelo Quattrociocchi,
According to stspin32f0b datasheet, USART serial interface is available via PB6 and PB7.
These pins are available on STEVAL-PTOOL1V1, J3 connector, pin15/17, refer to board schematic.