ST25 NFC/RFID tags and readers

Ask questions and find answers on ST25 NFC/RFID tags and readers, including connectivity implementations and antenna design.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Starting point RF-Field turned on X-Cube-NFC6

Hello everyone,I working with the X-Nucleo-NFC08A1 and the X-Cube-NFC6. I would like to know at what point in the program is the RF field turned on. The reason for this is that I would like to know how long a Tag has to be in the field to be ready fo...

Resolved! CR95HF on Arduino Uno Error 88

Hello,I am using the X-Nucleo-NFC03A1 shield with the Arduino Uno. I use the library for the BM019 as an inspiration for reading my tag. Setting the protocol, the echo command and the IDN command all work fine, but when I try to read the UID of the t...

Judith by Associate III
  • 3665 Views
  • 19 replies
  • 0 kudos

Resolved! How about STEVAL-SMARTAG1?

I have learned that STEVAL-SMARTAG1 can power MCU through EH of ST25 to achieve wireless transmission function, then can I replace the digital sensor with a thermocouple as a principle to collect data?

Resolved! M24LR with energy harvesting is possible?

Hi! I am a student new in this theme and i am searching for components to create a energy harvesting NFC system. This will work only with the power given by a mobile reader though the antenna. Searching for a dynamic tag, i have see that only M24LR a...

Ferga by Associate
  • 784 Views
  • 1 replies
  • 0 kudos

Resolved! Handling of Wait Time Extension (WTX)

Hi,In ST25RFAL library, version 2.8.0, in rfal_isoDep.c, function rfalIsoDepHandleControlMsg(), when ISODEP_S_WTX messages is handled, the code limits how many times a card can request wait time extension, specifically, this line:  if( (gIsoDep.cntSW...

DGabc.1 by Associate III
  • 857 Views
  • 1 replies
  • 1 kudos

Resolved! ST25R3911B-DISCO Implementing RFAL Library

Hello,I am trying to create an application that is able to use the ST25R3911B-DISCO to read ISO15693 tags. I read on the forums and understand that the reader does not natively support ISO15693 tags but that there is a RFAL library created by ST whic...

itsgimbi by Associate II
  • 872 Views
  • 1 replies
  • 0 kudos