User Activity

Hey,I am using the Nucleo-G474RE board with the X-Nucleo-NFC08A1 NFC Shield and use the X Cube NFC6 library in the Cube IDE environment. The initialization seems to work and there are no errors when building the code, but the demoCycle() function doe...
Hello,I am using the X-Nucleo-NFC03A1 shield with the Arduino Uno. I use the library for the BM019 as an inspiration for reading my tag. Setting the protocol, the echo command and the IDN command all work fine, but when I try to read the UID of the t...