ST25 NFC/RFID tags and readers

Ask questions and find answers on ST25 NFC/RFID tags and readers, including connectivity implementations and antenna design.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! RFID Multi tag reader

Hi,I am looking for an appropriate RFID reader IC for reading multiple tags simultaneously. The reader should be able to read 50-300 RFID stickers attached to packages stored in a container. Also the reader should cover a distance of 1m - 3m. Is ther...

shijomts by Associate
  • 1153 Views
  • 1 replies
  • 0 kudos

Resolved! STEVAL-253916B

I am looking for an HF reader board to which I can connect an external antenna.  I own the STEVAL-253916B and it might be possible to modify it to accomplish this but I can't locate the Gerber files on the ST website to make sure I'm doing it correct...

TedA by Associate II
  • 626 Views
  • 1 replies
  • 0 kudos

Resolved! Error while setting the ST25DV64KC NFC password

HelloWe are currently using ST25DV64KC nfc-v tags in our products, and found a possible bug during production.We set the NFC password in the last production step, using a self-developed android app (as, to my uderstanding, it cannot be done via i2C),...

GLeon.4 by Associate
  • 970 Views
  • 1 replies
  • 2 kudos

Resolved! Using AAT on NFC08a1

Hello everyone,I am using an NFC08A1 for my project and I would like to use the AAT. I roughly understand what happens in the AAT algorithm. However, I don't get any noticeable improvement when I apply it. The range in particular remains almost the s...

Resolved! Problem with the ST25RU3993-HPEV's FW

Hello everyone,I'm trying to compile the code wich is give at this address  on STM32CubeIDE and I have some problems when I want to compile the code. CubeIDE choose automaticalement the wrong "stm32l4xx_hal.h" and don't bring the one wich is in my wo...

ST.PNG
PRena.1 by Associate II
  • 639 Views
  • 1 replies
  • 0 kudos

Resolved! X-NUCLEO-NFC03A1 reading STEVAL-SMARTAG2

On both boards the demo application is installed, Oneshot on the STEVAL-SMARTAG2 and PollingTagDetect on the X-NUCLEO-NFC03A1. When using the STEVAL-SMARTAG2 without battery it can be read however I always see the same sensor data.  On the debug port...

Mark_MT by Associate II
  • 1018 Views
  • 3 replies
  • 0 kudos

Resolved! Using two X-NUCLEO-NFC08A1 with X-CUBE-NFC6

Hello everyone, for my project, I need to read a tag in two different places. Currently I am using an X-Nucleo-NFC08A1. I would like to add an additional X-Nucleo-NFC08A1 reader.The communication is done via SPI. What adjustments do I have to make in...

Resolved! NFC reader ST25R3916B EXT_LM pin

Hi,My application used ST25R3916B for transmit power for the card only.1. Is it possible to leave the EXT_LM pin unused or exclude external load modulation from my application?2. Can I use the testing point only on the pin EXT_LM pin?Best,Dalik LIM 

Dalik by Associate III
  • 719 Views
  • 1 replies
  • 1 kudos

Resolved! NFC Reader ST25R95

1. NFC ST25R95 Can I process if I don't use the MCU to control?2. Can I boot up voltage to 10V for pin TX1 and TX2 for differential pair?Best,Dalik

Dalik by Associate III
  • 3190 Views
  • 13 replies
  • 4 kudos