User Activity

I am looking for an HF reader board to which I can connect an external antenna.  I own the STEVAL-253916B and it might be possible to modify it to accomplish this but I can't locate the Gerber files on the ST website to make sure I'm doing it correct...
Figure 1 of the ST25R3918 spec shows an AGD pin in addition to the GND_A pin.   It is connected to VSS through two capacitors.  I don't see this pin on the Table 1 pin assignments.  What is the intention?Thanks,Ted
I want to use a MEMS oscillator driving the XTI pin instead of just a crystal between XTI and XTO.  What are the specifications on the input signal?  AC coupled? Amplitude? Drive impedance? Suggested circuit for a 0V to 3.3V output oscillator?
Where does the external pad get connected on the ST25R3918-AQWT package?  Ground?
Kudos given to