ST25 NFC/RFID tags and readers

Ask questions and find answers on ST25 NFC/RFID tags and readers, including connectivity implementations and antenna design.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Interfacing ST25RU3993 with TI micro-controller

Hi,I have purchased ST25RU3993-EVAL board with complete set and I am able to read tags. I would like to know if I can interface this board - RFID Reader with another micro controller (I wanted to interface with TI CC1352P1 launchpad), via SPI (or via...

SS1 by Associate II
  • 790 Views
  • 4 replies
  • 0 kudos

Resolved! ST25R3911B SPI Check

Hi , After starting power supply , without any configuration od ST25R3911B, can we directly read the "IC Identity Register 0x3F" just to check the SPI with the controller is working or not ? Will it give the value specified in the datasheet or should...

vaibh_p by Associate II
  • 733 Views
  • 3 replies
  • 0 kudos

Resolved! Correctly writing NDEF Text to ST25DV

I have ported the ST25DV NFC tag driver from STM SDK for TI's CC2650 SoC. Currently, I am able to successfully read and write TEXT data to the tag via I2C. However, when I read the data out from the tag using the STM's NFC Tap APP, I see that the da...

0690X00000BwM2nQAF.png

Resolved! Legacy libraries for NFC03A1 (CR95HF)

Hi Community, this is my first post here.I was wondering if there is a way to get the previous releases of the CUBE-NFC03A1 libraries (1.4.0 and lower). In fact, I want to use the Ndef_lib examples which are not supported anymore in the latest versio...

Resolved! How to receive more than 255 bytes of data via the fast transfer mailbox using the android St25 sdk?

Hi, I am attempting to receive a large amount of information via fast transfer mailbox on a ST25DV64K chip and and AndroidNFCReader using one mST25DVTag.writeMailboxMessage command, which commands the chip to send data continuously so long as it rece...

0690X00000Bx931QAB.png
KRa.1 by Associate
  • 955 Views
  • 2 replies
  • 0 kudos