ST25 NFC/RFID tags and readers

Ask questions and find answers on ST25 NFC/RFID tags and readers, including connectivity implementations and antenna design.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! what is the procedure to read ST25TA64K(NFC Forum Type 4 Tag,ISO/IEC 14443 Type A) Tag with NFC03A1 Reader and hosting MCU is STM32L452?

Dear all , My project is to read ST25TA64K(NFC Forum Type 4 Tag,ISO/IEC 14443 Type A) Tag with NFC03A1 Reader and hosting MCU is STM32L452.I am able to detect the Tag by Idle command.An wakeup event is getting occured after sending a...

PAkut.1 by Associate II
  • 574 Views
  • 2 replies
  • 0 kudos

Resolved! Is ST25 software library able to handle contactless memory with blocks of 2 bytes (for example SR176)?

Hello,in our project we need to handle the SR176 memory by the ST25r3911B component but we have some problems when we try to write the user blocks of the memory. We need also to handle the SRI512 card and we are able to write the blocks without probl...

ASiro.1 by Associate II
  • 979 Views
  • 5 replies
  • 0 kudos

Resolved! ST25TV Default Password

I have a ST25TV in the eSEAL Evaluation Board. I want to set the Counter Configuration. I need a password to do this (which I never set). What is the default password?Thanks,Vince

VColi.1 by Associate II
  • 874 Views
  • 1 replies
  • 0 kudos

Resolved! Is the version of STUHFL demo limited as compared to the one on windows? Multiple issues while building the demo for Linux.

Hi,I tried to follow the given instructions for building the STUHFL demo for linux but I encountered multiple issues:1) Header files were not found when building the solution.I added the absolute path in the settings of the project so that the header...

0690X00000D8CmAQAV.png
MStri.1 by Associate
  • 509 Views
  • 1 replies
  • 0 kudos

Resolved! At the product page for the ANT7-T-ST25DV04K Eval-Board there is an information that the board design and the Gerber files can be downloaded from www.st.com. Where can I find them?

This is the related page: https://www.st.com/content/st_com/en/products/evaluation-tools/product-evaluation-tools/st25-nfc-rfid-eval-tools/st25-nfc-rfid-antennas/ant7-t-st25dv04k.html

Resolved! RFAL Library

Should we have to necessarily use the RFAL library ? If not than can anybody tell the basic configurations of registers so that ST25R3911B detects TYPE-A card.

vaibh_p by Associate II
  • 630 Views
  • 1 replies
  • 0 kudos