Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! M9510-W data is not written correctly

I have a design that used an M95010-W and can read the Status as well as set the WEL bit and read it back in the status.  However when I try to write data starting at address 0 with the command string 0x02 0x00 followed by data in the same SPI frame ...

Resolved! How to load a firmware from M95P32 EEPROM ?

Hello,I need to and a FOTA to my application.I will receive the firmware with BLE and store it on M95P32 EEPROM. Then i need to load it on the mcu (STM32WL).I cannot find any example or resources that explain how can i  load a firmware from M95P32 EE...

malarab by Senior II
  • 1624 Views
  • 1 replies
  • 0 kudos

STA2500D - Alpwise BT Stack

Hi,I am looking for Alpwise BT Stack reference manual for STA2500D. Is there any info I can get regarding Alpwise BT stack? I am trying to check if we can modify the ACL packet data length 

SM R.1 by Associate
  • 1446 Views
  • 2 replies
  • 0 kudos

Need Reliability data for part SRC0GS22D

Hi, I require assistance in finding the reliability data for the products. I have search through the website but regrettably, I have not been able to find the required information. The components of interest are identified by the part numberSRC0GS22D...

WS2812B with STM8s003

Hello, I have bought an STM8s003 board and would like to use it to control ws2812B LEDs. But the libraries I have used with other controllers e.g. FastLED are not compatible with the STM8s003. Do you have any idea how I can solve this? I would prefer...

Erik1 by Associate
  • 6901 Views
  • 7 replies
  • 2 kudos