Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ST10F275 Access Protection

Hello CommunityI have somes mcu ST10F275 TQFP144 with Protection Access Enable  I need to disable protection   I only have Beeprog and ST10F programmer  I tried to write Access Protection Register using Beeprog programmer in order to disable protecti...

RS485 Transceiver ST485ERBDR

Hi,Iam using ST485ERBDR RS485 chip on my CNC controller card. In the datasheet I see that the Min data rate supported by the chip is 2.5Mbps.Please can anyone confirm what is the max Data rate it supports.

Resolved! ST10F252-ABG

I know that this IC: ST10F252-ABG is old, but is there any cross or direct replacement for it?Thanks,Byron

ATS-Byron by Associate II
  • 1680 Views
  • 2 replies
  • 1 kudos

PSpice Model of Viper Series

Posted on September 03, 2015 at 12:41Dear all,I would like to export the current design project by Viper06 and Viper16 to PSpice, but the ''export button'' is greyed...In your eDesignSuite Video, you also explain the ''save functions''  with a Viper...

Resolved! L9735TR

Do you have a data sheet for this product? Has this product been discontinued? Is there a reference for alternative part numbers

xuzejian by Associate II
  • 1832 Views
  • 3 replies
  • 2 kudos

TL062 Pspice model

Hi everyone,I am working on a LTSPICE model for TL062 I think maybe you can help me :)This is the schematic diagram is the datasheet :and this is my spice model To test if my amplifier is working i am trying the basic utilisation for OpAmp : So I con...

fru999_0-1714486095109.png fru999_2-1714486206089.png fru999_3-1714486250161.png fru999_1-1714486147052.png
fru999 by Associate III
  • 2293 Views
  • 2 replies
  • 0 kudos

Resolved! STM8L151C8U6

Hello , Can you help me for the microntroleur reference 1) Why don't you recommend this product for new designs ?2) Do you have an idea of the number of years before the end of its life ?3) NRND information available in an PCN ? Thank you in advance

sguec.1 by Associate II
  • 4292 Views
  • 6 replies
  • 0 kudos

STVD setup

I changed my laptop system from "Windows 7" to "Windows 10" and reinstalled "STVD", "STVP", "COSMIC Software". When I try to set the toolset in the "STVD" window for "STM8 Cosmic", the root path "C:\Program Files (x86)\COSMIC\FSE_Compilers\CXSTM8" an...