2023-04-01 5:21 PM
TS3011 pspice file posted on the ST website cannot translate to ADS. The file shows ten pin circuits after translation, while the device only has five pins
2023-04-02 12:37 PM
Welcome, @RA2, to the community!
You unfortunately had a typo and I took the liberty of changing the device name to the correct TS3011 if that's OK with you?
Sorry you are having problems with the conversion. However, this seems to be a problem of ADS, because in the SPICE model only 5 pins are clearly mentioned:
************ CONNECTIONS:
**** NON-INVERTING INPUT
**** | INVERTING INPUT
**** | | POSITIVE POWER SUPPLY
**** | | | NEGATIVE POWER SUPPLY
**** | | | | OUTPUT
**** | | | | |
**** | | | | |
.SUBCKT TS3011 VP VM VCCP VCCN VSMaybe Keysight Technologies support can help you?
Regards
/Peter