Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Replacement for BMO055

Dear forumI need to update a board that uses BMO055 9 axis IMU and I need to know what is the preferred ST solution that best fit this obsoleted part.I need the 3 axis gyro + 3axis accelerometer + 3 axis magnetometerIf there is a single chip solution...

nachus001 by Associate II
  • 2666 Views
  • 6 replies
  • 0 kudos

M41ST87W RTC Module Read problem

We use M41ST87W as RTC module. We set the stop bit (ST) to 0. We can also observe the frequency at the F32K output. We constantly read the Second register but we do not see any change. What could be the reason for this?

elehab by Associate
  • 1045 Views
  • 2 replies
  • 0 kudos

Resolved! COREMP135 software

I purchase one M5STAck COREMP135, it noticed work for linux, but when I use the software, it can't handle user account , only use root login.Then I try build image by myself, the github support was 2-3 years ago.I see one training company - Bootlin s...

ST-LINK V2 windows 10

Hello ,  I have 5 ST-LINK/V2 and 5 products. Each programmer is connected to one product at a time. I am using Windows 7 and a USB hub. Everything works fine, but when I migrated to Windows 10, I encountered an unstable programming issue. I updated t...

Resolved! STM8S003F3 Datasheet pin description

I'm just starting to learn about MCUs and am reviewing the datasheet for the STM8S003F3. In the pin description table, I came across some symbols that I'm not quite sure about, such as bold X with underline (X), regular X (X), and dash (-). What do t...

pin_description.png
zin10 by Associate II
  • 2131 Views
  • 4 replies
  • 2 kudos

HSO with flux weakening

I designed hardware by myself and used MCSDK 6.3.2. I chose HSO algorithm in Workbench, this work well except flux weakening feature is missing. So we cannot run motor with full load. Please advise how we can config Workbench to use HSO together with...

intania by Associate
  • 841 Views
  • 0 replies
  • 0 kudos

Resolved! STP24DP05 IC queries

Best SPI Routing Method for Double-Sided 16×128 LED Matrix Using STP24DP05Project OverviewI am designing a double-sided 16×128 RGB LED matrix display using STP24DP05 LED drivers. The LED drivers are controlled using a single SPI bus from the MCU. Sin...

clintt by Associate II
  • 2383 Views
  • 4 replies
  • 1 kudos