User Activity

I have multiple issues to report with the MC Workbench (MCWB). I am using Version 6.3.2 and trying to get a dual motor BLDC setup working on custom hardware.In the .zip-file there is a minimal project required for viewing the issues and additionally ...
Hello ST Community, I am using a VNHD7008AY ICs to control a brushed motor (XDW043003-01, LowSide-Mosfets: SIR606DP-T1-GE3CT)The PCB is supplied with 24VDC. The application has the problem, that the motor can be moved by the user both in and against ...