Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! RBO40

Hello, I am trying to build a power supply to power a vehicle tracker.  Can I use two RBO40 in series, so the output of first RBO40 connected to input of second RBO40?  Reason, when a thief steals a vehicle they want to stop the tracker working and s...

Padg by Associate
  • 1495 Views
  • 3 replies
  • 1 kudos

Resolved! Thermal Resistance of L6201PS on FR4 PCB ?

I am writing to inquire about the thermal resistance of the L6201PS. The datasheet provides information on the thermal resistance for an aluminum PCB, but I need to know the thermal resistance when using a glass epoxy (FR4) PCB.Could you please provi...

takumi by Associate II
  • 2111 Views
  • 5 replies
  • 2 kudos

Resolved! STLUX adc trigger

I am trying to configure an STLUX285 SMED to trigger an ADC measurement but am unable to find the documentation of the registers required to do this.RM0380 claims "SMED as ADC trigger source" in section 21.16."AFR_IOMXP2" is supposed to have a bit ca...

mschn.17 by Associate II
  • 1121 Views
  • 1 replies
  • 0 kudos

Need help with STM32U5 and SPI

Hi Folks:I have this Riverdi board (RVT50HQSNWC00) with a STM32U5A9NJH6Q MCU.I want to programming data transmission according to the image attached Im intent to use SPI but if any better option let me knowthanks in advance   

IMG-4286.jpg
VSANGIL by Associate II
  • 1846 Views
  • 4 replies
  • 1 kudos

How To get internal RTC time using STM8L050J3

Hi All,  We are using the STM8L050J3 chip and trying to get time using an internal RTC with LSI. We are getting some responses but are not sure what it is. Here is our result (TIME: 3108:4877:2644) and code. We are using the cosmic compiler. Could an...

Cpg2 by Associate II
  • 1673 Views
  • 3 replies
  • 0 kudos