Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32 blue pill, SPI mcu-mcu comunication

Hello everyone. I'm currently just learning and getting familiar with microcontrollers. For educational purposes, I would like to set up master-slave communication between two C8T6 boards. The master should send an array of values, which the slave re...

Resolved! M24512-A125

I intended to write a wrapper to access the memory section of the M24512 part. I began with enumeration using the device identification code, but instead of receiving I2C Family as 0xE0, I got 0xFF, I need to understand what went wrong. Additionally,...

Read-Byte.png Write-Byte.png Wrong-Family-Code.png
pratap by Associate
  • 903 Views
  • 2 replies
  • 0 kudos

Resolved! "NO DEVICE FOUND ON TARGET"

and in the FAIL.txt "The interface firmware FAILED to reset/halt the target MCU" When I connected my F4 Discovery card to my computer, the card's folder opened in front of me and in it, apart from the usual files, another file called FAIL.txt, which ...

Morpheuss01_0-1746033644852.png

Resolved! Ethernet tool to analysis

Hi I am trying to communicate via ethernet on STm32f407 board with phy LAN8720. I have used TCP protocol and I have used Hercules for sending and reciving frame. But I want to acheive the operation sung HAL_ETH_Transmit (I want to send raw ethernet f...

Ash1 by Associate III
  • 2567 Views
  • 7 replies
  • 3 kudos