Skip to main content
Senior III
May 5, 2025
Solved

SPI issue keep getting 0 values from accelerometer

  • May 5, 2025
  • 16 replies
  • 1449 views

NUCLEO-WB55RG communicating via SPI1 to an ADXL362 eval board
I set up the project (attched below) using CubeIDE, generated the code & placed my own callbacks for the SPI in main.

When I look at the value for the Z direction I should be getting a value that indicates roughly 1g but all I get is 0. The same for all the other axis, no change in any value no matter how I orient the sensor.

To check that the acceleromter was working I hooked it up to an Arduino using a 3rd party library especially for the ADXL362. That all worked as expected, so I know the accelerometer is working.

When I go through the code with the debugger it doesn't hang anywhere so I'm guessing my callbacks are working, its just I dont get any data back, all values remain at 0

Anyone see anything obvious that I'm doing wrong?

This topic has been closed for replies.
Best answer by NicRoberts

Found it!!
I had configured PA4 as SPI1_NSS as soon as I reconfigured it as a GPIO output it all worked fine.

Thanks fellas for walking me through the debugging of this.

16 replies

Tesla DeLorean
Guru
May 5, 2025

Check if Arduino Library is doing something to initialize/start the accelerometer. I remember the Bosch devices needing a quick magic sequence and scale selection. 

Get a scope or logic analyzer on the pins and review working and non-working signals.

Link to github library for working driver you're using / attempting to port

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Senior III
May 6, 2025

The Arduino library I used Winkelict ADXL362 Arduino library 

The only thing I've spotted is that they do is a soft reset first, which I've now added to ADXL362_Init()

 

SPI_WriteRegister(ADXL362_SOFT_RESET, 0x52);
HAL_Delay(500);

Which doesn't change the behaviour, I still get 0 readings.

I changed the power control register to disable auto-sleep and remain in measurement mode

SPI_WriteRegister(ADXL362_POWER_CTL, 0x02);

Still no readings. So I decided to check if I could even read the chip ID, I cant I just get a value of 0.

Andrew Neil
Super User
May 6, 2025

To prove basic SPI comms, can you successfully read the Device ID register ?

As @Tesla DeLorean said, use a scope and/or logic analyser to verify comms - compare & contrast with the Arduino.

 

Have you checked the AD Product Page:

https://www.analog.com/en/products/adxl362.html#:~:text=Sheet%20(Rev.%20G)-,Software%20Resources,-All

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Senior III
May 6, 2025

Not even getting the device ID. 

Yes I have the device datasheet with the register map & the SPI settings.

As soon as I get a working scope I'll check the comms.

Senior III
May 7, 2025

NicRoberts_0-1746628062676.png

From the scope, top row is from the STM32WB55, bottom row from the Arduino.

Channel 1 - top trace is the CS line. I couldn't get a reading of the clock & the CS line one the Arduino, as soon as I probed SCLK then the chip errored out and just returned 0s & the clock & CS traces interfered with each other..

 

The STM MISO line is always 0 no matter what command I send, so no ID, no axis data, always 0. 

I notice the CS line has that blip which I assume is the gap between bytes being sent?

SCLK is bang on 4MHz

Andrew Neil
Super User
May 7, 2025

Does your scope not have a trace capture or screenshot facility?

 


@NicRoberts wrote:

I notice the CS line has that blip which I assume is the gap between bytes being sent?


Looks like it.

That'll be (at least one reason) why it's not working - CS should stay low for the entire transaction:

AndrewNeil_0-1746629677738.png

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Senior III
May 7, 2025

@Andrew Neil wrote:

Does your scope not have a trace capture or screenshot facility?


It doesnt even have a USB port :D just an old school parallel port.

 


That'll be (at least one reason) why it's not working - CS should stay low for the entire transaction:

 


 Yeah that's what I was expecting.  I cant see it in the code unless the CS is being taken care of in the HAL & I shouldn't be setting & resetting it in my ADXL362 driver?

Senior III
May 8, 2025

Frustratingly the SPI call backs dont work in the debugger so they just hang which doesn't happen when its just running.

Anyway, it looks like I have no control over the CS line (PA4). When I clock through the code in the debugger & get to the line,

HAL_GPIO_WritePin(ADXL_GPIO_Port, ADXLCS_Pin, GPIO_PIN_RESET);

 The trace on that pin stays HI only when,

HAL_SPI_Transmit_DMA(adxlParams.hspi, command_address, 2);

is called does the CS line get pulled LO & then it exhibits the behaviour above, i.e. the CS line goes HI between each byte sent. I cant find anywhere in the HAL_SPI_Transmit_DMA() function that is acting on PA4, so that's puzzling.

So I've tried to just toggle PA4 in main() in the while() loop

HAL_GPIO_WritePin(ADXLCS_GPIO_Port, ADXLCS_Pin, GPIO_PIN_RESET);
HAL_Delay(500);
HAL_GPIO_WritePin(ADXLCS_GPIO_Port, ADXLCS_Pin, GPIO_PIN_SET);

It just stays HI

// Pin & GPIO port defines in ADXL362.h
#define ADXLCS_Pin PIN_4
#define ADXLCS_GPIO_Port GPIOA

 

NicRobertsAuthorBest answer
Senior III
May 8, 2025

Found it!!
I had configured PA4 as SPI1_NSS as soon as I reconfigured it as a GPIO output it all worked fine.

Thanks fellas for walking me through the debugging of this.